2010-07-19 4:25 AM
TIM4 PWM Out
2011-05-17 4:59 AM
This worked for Timer1. Do you need to use function, TIM_CtrlPWMOutputs(TIMx, ENABLE) ?
John F. #include ''stm32f10x.h'' void RCC_Configuration(void); void GPIO_Configuration(void); void Timer1_Configuration(void); //note with SYSCLK_FREQ_72MHz defined, PCLK1 = 36MHz and PCLK2 = 72MHz uint16_t CCR1_Val = 1000; //1500 = 1.5ms (1000 = 1ms, 2000 = 2ms); int main(void) { RCC_Configuration(); GPIO_Configuration(); Timer1_Configuration(); while(1) { GPIO_WriteBit(GPIOB, GPIO_Pin_0, Bit_SET); GPIO_WriteBit(GPIOB, GPIO_Pin_0, Bit_RESET); } } void RCC_Configuration(void) { //Setup the microcontroller system. Initialize the Embedded Flash Interface, //initialize the PLL and update the SystemFrequency variable. SystemInit(); // Enable GPIOB, AFIO and Timer1 clocks RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO | RCC_APB2Periph_TIM1, ENABLE); } void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; //partial remap of Timer1 GPIO_PinRemapConfig(GPIO_PartialRemap_TIM1, ENABLE); //GPIOB Configuration: TIM1 channel 2N as alternate function push-pull GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); } void Timer1_Configuration(void) { //Timer1 is clocked by PCLK2 = 72MHz TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; TIM_DeInit(TIM1); //Time base configuration TIM_TimeBaseStructure.TIM_Prescaler = 71; //clocked at 72MHz / 72 = 1MHz TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 19999; //period = (72MHz / 72) / 20000 = 50Hz (20ms period) TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Channel 1 Configuration in PWM mode */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset; TIM_OC2Init(TIM1, &TIM_OCInitStructure); TIM_OC2PreloadConfig(TIM1, TIM_OCPreload_Enable); TIM_CtrlPWMOutputs(TIM1, ENABLE); //TIM1 enable counter TIM_Cmd(TIM1, ENABLE); }2011-05-17 4:59 AM
You only need that for Timers 1 and 8 (if present). You do, however, need to enable the GPIO port, alternate function and timer clocks though.
2011-05-17 4:59 AM
Thank You, PWM1 is working
2011-05-17 4:59 AM
Hello Mr. John F.
Im using the same code to generate a PWM that you posted here but i can`t get any signal. I want to use it to control a RGB LED so i changed the GPIO configuration but i cant get any signal... is there anything else i need to do it? Thank youWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.