2010-07-19 5:28 AM
Timer Period
2011-05-17 4:59 AM
Hi diez,
What do you mean by ''Timer Frecuency: 2KHz'' ? Is it the system clock that was 72 MHz in ST example ? MCU Lüfter2011-05-17 4:59 AM
I often refer to Freq timer Tim = 1/Tim.
Tim being the time it takes to overflow the timer
2011-05-17 4:59 AM
TIM1_Prescaler: 7200 (7199+1)
TIM1_Period: 1
TIM1_RepetitionCounter: 0 This values are invalid with the formula. This Value of Tim1 Frec=2KHz, and Tim1period=1/2KHz-->0,5mSeg. I had got changing prescaler,period and repetition counter
2011-05-17 4:59 AM
First of all, thks for your quick response.
What is your sysclk frequency? 72MHzWhat is the measured frequency?Timer Frecuency: 2KHzTIM1_Prescaler: 3600 (3599+1)
TIM1_Period: 1
TIM1_RepetitionCounter: 4
What is the calculated frequency? I Don´t understand What is the complete timer initialization code? /* ============================================================================= * Function Name : CLK_configuration * Description : Configuración del Nested vectored interrupt. ============================================================================= */ void CLK_configuration (void) { /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ HSI RC (8 MHz) ~~~~ */ RCC_HSICmd(ENABLE); /* ENABLE/DISABLE RCC_CR.HSION */ while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET); /* WAIT TO HARDWARE OFF */ RCC_SYSCLKConfig(RCC_SYSCLKSource_HSI); /* MODIFICA RCC_CFGR.SW */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ HSE_Value (8 MHz) stm32f10x_conf.h ~~~~ */ RCC_HSEConfig(RCC_HSE_ON); /* ON/OFF RCC_CR.HSEON */ while(RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET); /* WAIT TO HARDWARE OFF */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ PHASE LOOP LOCKED PLLCLK->72MHz ~~~~ */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9); /* RCC_CFGR.PLLSRC=1, RCC_CFGR.PLLXRPRE=0 y RCC_CFGR.PLLMULL=0111 */ RCC_PLLCmd(ENABLE); /* ENABLE/DISABLE RCC_CR.PLLON */ while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); /* WAIT TO HARDWARE OFF */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ SYSTEM CLOCK SYSCLK=72MHZ HCLK=72MHZ ~~~~ */ RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5); /* 72MHz/1.5=48MHZ */ RCC_ADCCLKConfig(RCC_PCLK2_Div8); /* CONFIGURE RCC_CFGR.ADCPRE */ RCC_PCLK2Config(RCC_HCLK_Div1); /* CONFIGURE RCC_CFGR.PPRE2 APB2 PCLK2=72MHz */ RCC_PCLK1Config(RCC_HCLK_Div2); /* CONFIGURE RCC_CFGR.PPRE1 */ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* CONFIGURE RCC_CFGR.HPRE */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ EMB_FLASH ~~~~ */ #ifdef EMB_FLASH // 5. Init Embedded Flash // Zero wait state, if 0 < HCLK 24 MHz // One wait state, if 24 MHz < HCLK 56 MHz // Two wait states, if 56 MHz < HCLK 72 MHz // Flash wait state FLASH_SetLatency(FLASH_Latency_2); // Half cycle access FLASH_HalfCycleAccessCmd(FLASH_HalfCycleAccess_Disable); // Prefetch buffer FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); #endif // EMB_FLASH /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ // 5. Clock system from PLL RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* MODIFICA RCC_CFGR.SW */ } /* ============================================================================= * Function Name : TIMER_configuration * Description : Configuración del TIMER. ============================================================================= */ void TIMER_configuration(void) { TIM1_TimeBaseInitTypeDef TIM1_TimeBaseInitStruct; /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ TIM1 INIT ~~~ */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1,ENABLE); /* RCC_APB2ENR.TIM1EN ENABLE CLK TIM1 */ RCC_APB2PeriphResetCmd(RCC_APB2Periph_TIM1,DISABLE); /* RCC_APB2RSTR.TIM1RST RESET TIM1 */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ CONFIGURACION TIM1 ~~ */
#define Prescala 3600 /* Maximo 65536 */ #define Periodo 1 /* Maximo 65536 */ #define Repeticion 5 /* Maximo 256 */ TIM1_TimeBaseInitStruct.TIM1_Prescaler = Prescala-1; /* PRESCALER TIMx_PSC */ TIM1_TimeBaseInitStruct.TIM1_CounterMode = TIM1_CounterMode_Up; /* TIM1_CR1.DIR */ TIM1_TimeBaseInitStruct.TIM1_Period = Periodo; /* PERIOD TIMx_ARR */ TIM1_TimeBaseInitStruct.TIM1_ClockDivision = TIM1_CKD_DIV1; /* TIM1_CR1.CKD */ TIM1_TimeBaseInitStruct.TIM1_RepetitionCounter = 0; /* TIM1_RCR */ TIM1_TimeBaseInit(&TIM1_TimeBaseInitStruct); // Clear update interrupt bit TIM1_ClearITPendingBit(TIM1_FLAG_Update); // Enable update interrupt TIM1_ITConfig(TIM1_FLAG_Update,ENABLE); // Enable timer counting TIM1_Cmd(ENABLE); }
2011-05-17 4:59 AM
Your text is a little bit unclear to me.
What is your sysclk frequency? What is the measured frequency? What is the calculated frequency? What is the complete timer initialization code? BTW: For many frequencies you have many possibilities to achieve them, but some combinations seem not to function. I don't know why. I have checked the limits of the values and the manual. Greater and lower combinations run, several between not. Inspiring confidencehttp://dict.leo.org/ende?lp=ende&p=Ci4HO3kMAA&search=inspiring&trestr=0x8004
;)2011-05-17 4:59 AM
2011-05-17 4:59 AM
How did you measure the values?
The calculated frequency for your code is: f_tim = 72.000.000Hz/(3599+1)/(1+1)= 10.000 Hz I would NOT use values lower than 3 for TIM_TimeBaseInitStruct->TIM_Period. The manual does not warn, but i do it. The timer seems to be special featured with those values. BTW: Did you see, that you don't use your defintion for TIM_TimeBaseInitStruct->TIM_RepetitionCounter?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.