2008-04-27 11:19 PM
TIM4 do not work in STM32F103V8T6
2011-05-17 3:31 AM
Hy!
i try to use timer 4 (TIM4) in my project, but it doesn't work. Till now i tried all other timers (Timer1, Timer2&3) and they are working fine. I used the same initialization routines for Timer4 as for the others:Code:
// TIM4 clock enable 24MHz RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); // Time base configuration TIM_TimeBaseStructure.TIM_Period = TIM4_Freq_16kHz; TIM_TimeBaseStructure.TIM_Prescaler = 1; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); TIM_ITConfig(TIM4,TIM_IT_Update, ENABLE); // Enable TIM4 global Interrupt NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // TIM enable counter TIM_Cmd(TIM4, ENABLE); Timer 4 should be available in this device (described in the datasheet). µC: STM32F103V8 IAR Embedded Workbench IDE JLINK for ARM processors Does anybody knows this issue or knows what happens with TIM4 in this device???2011-05-17 3:31 AM
Take a look at this line of your code
NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQChannel; You have enabled the TIM3 interrupt not Timer 4 This could be a problem....2011-05-17 3:31 AM
hy!
i know, my fault, i copied the wrong part of my code. I tried to initialize all 4 timers. 1 - 3 worked fine, only 4th doesn't work. I took a look at the registers of TIM4 with the debugger when this line appearsCode:
TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);
and nothing happens there. it looks like TIM4 isn't there! whole code is now:Code:
// TIM4 clock enable 24MHz RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); // Time base configuration TIM_TimeBaseStructure.TIM_Period = TIM4_Freq_16kHz; TIM_TimeBaseStructure.TIM_Prescaler = 1; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); TIM_ITConfig(TIM4,TIM_IT_Update, ENABLE); // Enable TIM4 global Interrupt NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // TIM enable counter TIM_Cmd(TIM4, ENABLE);2011-05-17 3:31 AM
can you try the TIM example 8 from the ''ARM-based 32-bit MCU STM32F101xx and STM32F103xx firmware library''. It uses the TIM4 and it works fine.
http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=110#Firmware2011-05-17 3:31 AM
i tried the example 8 with the ''GettingStarted'' workspace for IAR Workbench, and it works!
i also checked the registers for TIM4 with debugger and the output pin channel1 of tim4. it worked fine. so i checked all my project settings, and did changes at the DEBUGGER -> DOWNLOAD -> Flash loader file. this was set to ''$TOOLKIT_DIR$\config\flashloader\ST\FlashSTM32F10x.d79'' manually. i changed it to the ''Default'' setting like in the working workspace (TIM4 example), and now i get crazy errors: Fri Apr 25 15:20:26 2008: DLL version: V3.80c, compiled Apr 9 2008 18:56:00 Fri Apr 25 15:20:26 2008: Firmware: J-Link ARM V6 compiled Mar 3 2008 18:04:42 Fri Apr 25 15:20:26 2008: JTAG speed is initially set to: 32 kHz Fri Apr 25 15:20:26 2008: TotalIRLen = 9, IRPrint = 0x0011 Fri Apr 25 15:20:26 2008: Found Cortex-M3, Little endian. Fri Apr 25 15:20:26 2008: TPIU fitted. Fri Apr 25 15:20:26 2008: FPUnit: 6 code (BP) slots and 2 literal slots Fri Apr 25 15:20:26 2008: Hardware reset with strategy 1 was performed Fri Apr 25 15:20:26 2008: Initial reset was performed Fri Apr 25 15:20:26 2008: J-Link found 2 JTAG devices. ARM core Id: 3BA00477(Cortex M3), ARM core Id: 00000000(ARM9) Fri Apr 25 15:20:26 2008: Device at TAP0 selected Fri Apr 25 15:20:28 2008: 3518 bytes downloaded and verified (2.36 Kbytes/sec) Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000168, target byte: 0x00, byte in file: 0x09 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000169, target byte: 0x00, byte in file: 0x68 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000016A, target byte: 0x00, byte in file: 0x51 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000016B, target byte: 0x00, byte in file: 0xF0 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000016C, target byte: 0xBE, byte in file: 0x04 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000016D, target byte: 0x0A, byte in file: 0x01 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000016E, target byte: 0x00, byte in file: 0x01 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000016F, target byte: 0x00, byte in file: 0x60 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000170, target byte: 0x32, byte in file: 0x06 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000171, target byte: 0x0C, byte in file: 0x48 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000172, target byte: 0x00, byte in file: 0x06 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000173, target byte: 0x00, byte in file: 0x49 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000174, target byte: 0x04, byte in file: 0x09 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000175, target byte: 0x0A, byte in file: 0x68 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000176, target byte: 0x00, byte in file: 0x01 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000177, target byte: 0x00, byte in file: 0x22 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000178, target byte: 0xD6, byte in file: 0x91 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x20000179, target byte: 0x02, byte in file: 0x43 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000017A, target byte: 0x00, byte in file: 0x01 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000017B, target byte: 0x00, byte in file: 0x60 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000017C, target byte: 0x1F, byte in file: 0x24 Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000017D, target byte: 0x0F, byte in file: 0x1D Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000017E, target byte: 0x00, byte in file: 0x3F Fri Apr 25 15:20:28 2008: Warning: Verify error at address 0x2000017F, target byte: 0x00, byte in file: 0x1D Fri Apr 25 15:20:28 2008: There were warnings during download of FLASH loader, see Log Window Fri Apr 25 15:20:29 2008: Failed to load flash loader: C:\Programme\IAR Systems\Embedded Workbench 4.0 Kickstart\arm\config\flashloader\ST\FlashSTM32F10x.d79 When i try to change to the settings before, the same error occurs. i don't know what to do now. i tried 2 boards with my described processor type, and the IAR kickstart kit board, nothing helps!!!2011-05-17 3:31 AM
Can you share your project
2011-05-17 3:31 AM
hy!
in principle its the same code like in the ''getting started'' example, only with the Example 8 files included. with my company project i started also with the ''gettingStarted''. Following peripherals are in use: ADC with DMA I2C for Display I2C for Flash TIM1 to 3 and some GPIO for keyboard etc. i recognized the first problems since i included the ADC with DMA! i don't know if this could be the problem2011-05-17 3:31 AM
Hy!
Today i did some other tests with my software. i took another (unflashed) board, and tried my software without enabling the ADC with DMA. the flashing and debugging with ''IAR workbench'' worked fine! i repeated that procedure several times without any problem. Than i tried to enable the ADC with DMA. The first programming (flashing) was done correctly and all works fine. but when i try to flash again the same software the described errors appear. What could be the problem??? my ADC init routine:Code:
void Analog_Init(void) { // Enable DMA clock RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA, ENABLE); // Enable ADC1 and GPIOC clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_GPIOC, ENABLE); // DMA channel1 configuration ---------------------------------------------- DMA_DeInit(DMA_Channel1); DMA_InitStructure.DMA_PeripheralBaseAddr = (u32)ADC1_DR_Address; DMA_InitStructure.DMA_MemoryBaseAddr = (u32)ADC_ConvertedValueTab; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = 6; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA_Channel1, &DMA_InitStructure); // Enable DMA Channel1 DMA_Cmd(DMA_Channel1, ENABLE); // ADC1 configuration ------------------------------------------------------ ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfChannel = 6; ADC_Init(ADC1, &ADC_InitStructure); // ADC1 regular channels configuration ADC_RegularChannelConfig(ADC1, ADC_Channel_10, 1, ADC_SampleTime_239Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 2, ADC_SampleTime_239Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 3, ADC_SampleTime_239Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_13, 4, ADC_SampleTime_239Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 5, ADC_SampleTime_239Cycles5); ADC_RegularChannelConfig(ADC1, ADC_Channel_15, 6, ADC_SampleTime_239Cycles5); // Enable ADC1 DMA ADC_DMACmd(ADC1, ENABLE); // Enable ADC1 ADC_Cmd(ADC1, ENABLE); // Enable ADC1 reset calibaration register ADC_ResetCalibration(ADC1); // Check the end of ADC1 reset calibration register while(ADC_GetResetCalibrationStatus(ADC1)); // Start ADC1 calibaration ADC_StartCalibration(ADC1); // Check the end of ADC1 calibration while(ADC_GetCalibrationStatus(ADC1)); // Start ADC1 Software Conversion ADC_SoftwareStartConvCmd(ADC1, ENABLE); }2011-05-17 3:31 AM
To avoid this problem try to reconfigure your project as in the attached image
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.