2025-04-27 3:45 AM - last edited on 2025-05-01 7:40 AM by Andrew Neil
Hi,
I'm working on an STM32F303RE project.
So far, only the UART and TIM3 are working properly.
I successfully configured TIM3 in PWM mode on 3 channels, and everything runs as expected. Project is build only on CMSIS libirary.
void clock_config(void)
{
RCC->CR |= RCC_CR_HSION;
while (!(RCC->CR & RCC_CR_HSIRDY));
// RCC->CR |= RCC_CFGR_PLLSRC
RCC->APB1ENR |= RCC_APB1ENR_PWREN;
RCC->CFGR |= RCC_CFGR_HPRE_DIV1;
RCC->CFGR|= RCC_CFGR_PPRE1_DIV2;
//PPL SOURCE MUX
// RCC->CFGR |= RCC_CFGR_PLLMUL9;
RCC->CFGR |= (0x7 << RCC_CFGR_PLLMUL_Pos);
RCC->CR |= RCC_CR_PLLON;
while (!(RCC->CR & RCC_CR_PLLRDY));
RCC->CFGR |= RCC_CFGR_SW_PLL;
while(!(RCC->CFGR & RCC_CFGR_SWS));
RCC -> AHBENR |= RCC_AHBENR_GPIOAEN;
RCC -> AHBENR |= RCC_AHBENR_GPIOBEN;
}
void TIM3_IRQHandler(void)
{
if (TIM3->SR & TIM_SR_CC1IF)
{
TIM3->SR &= ~TIM_SR_CC1IF; // Wyczyść flagę
GPIOA->ODR ^= GPIO_ODR_6; // Przełącz PA6 (D12) z
}
}
void TIM2_IRQHandler(void)
{
//PA0 a0
if (TIM2->SR & TIM_SR_CC1IF)
{
TIM2->SR &= ~TIM_SR_CC1IF; // Wyczyść flagę
GPIOA->ODR ^= GPIO_ODR_0; // Przełącz A0 y
}
}
void TIM4_IRQHandler(void)
{
if (TIM4->SR & TIM_SR_CC1IF)
{
TIM4->SR &= ~TIM_SR_CC1IF; // Wyczyść flagę
GPIOA->ODR ^= GPIO_ODR_11; // Przełącz (PA11) x
}
}
void DIRconfig_x(void)
{
GPIOB -> MODER |= GPIO_MODER_MODER6_0;
GPIOB -> MODER &= ~(GPIO_MODER_MODER6_1);
GPIOB -> OTYPER &= ~(GPIO_OTYPER_OT_6);
GPIOB -> OSPEEDR &= ~(GPIO_OSPEEDER_OSPEEDR6);
GPIOB -> PUPDR &= ~(GPIO_PUPDR_PUPDR6);
}
void configure_z_TIMER3(void)
{
//PA6:D12 CH1
RCC -> APB1ENR |= RCC_APB1ENR_TIM3EN;
TIM3->PSC = 1999; //72mghz 32??
TIM3->ARR = 19; //PA6
TIM3->CR1 |= TIM_CR1_ARPE;
GPIOA->MODER |= GPIO_MODER_MODER6_0;
TIM3->CNT=0;
TIM3->CCMR1 |= (TIM_CCMR1_OC1M_0 | TIM_CCMR1_OC1M_1); //outputcomare config
TIM3->CCER |= TIM_CCER_CC1E;
//interuptTIM3
TIM3 -> DIER |= TIM_DIER_UIE;
TIM3 -> DIER |= TIM_DIER_CC1IE;
NVIC_SetPriority(TIM3_IRQn, 1);
NVIC_EnableIRQ(TIM3_IRQn);
TIM3->CR1|= TIM_CR1_CEN;
}
void configure_y_TIMER2(void)
{
//PA0:A0 AF1
RCC -> APB1ENR |= RCC_APB1ENR_TIM2EN;
TIM2->PSC = 7199; //72mghz 32??
TIM2->ARR = 19;
TIM2->CR1 |= TIM_CR1_ARPE;
GPIOA->MODER |= GPIO_MODER_MODER0_0;
GPIOA->AFR[0] |= ((0x1 << GPIO_AFRL_AFRL0_Pos));
TIM2->CNT=0;
TIM2->CCMR1 |= (TIM_CCMR1_OC1M_0 | TIM_CCMR1_OC1M_1); //outputcomare config
TIM2->CCER |= TIM_CCER_CC1E;
//interuptTIM3
TIM2 -> DIER |= TIM_DIER_UIE;
TIM2 -> DIER |= TIM_DIER_CC1IE;
NVIC_SetPriority(TIM2_IRQn, 3);
NVIC_EnableIRQ(TIM2_IRQn);
TIM2->CR1|= TIM_CR1_CEN;
}
void configure_x_TIMER4(void)
{
//PA11:D12
RCC -> APB1ENR |= RCC_APB1ENR_TIM4EN;
TIM4->PSC = 7199; //72mghz 32??
TIM4->ARR = 19; //PA6
TIM4->CR1 |= TIM_CR1_ARPE;
GPIOA->MODER |= GPIO_MODER_MODER11_0;
TIM1->CNT=0;
TIM4->CCMR1 |= (TIM_CCMR1_OC1M_0 | TIM_CCMR1_OC1M_1); //outputcomare config
TIM4->CCER |= TIM_CCER_CC1E;
//interuptTIM3
TIM4 -> DIER |= TIM_DIER_UIE;
TIM4 -> DIER |= TIM_DIER_CC1IE;
NVIC_SetPriority(TIM4_IRQn, 2);
NVIC_EnableIRQ(TIM4_IRQn);
TIM4->CR1|= TIM_CR1_CEN;
}
int main(void)
{
clock_config();
SysTick_Config(72000000/1);
config_UART();
configure_z_TIMER3();
configure_y_TIMER2();
configure_x_TIMER4();
DIRconfig_x();
USART2->TDR = 'D';
while (!(USART2->ISR & USART_ISR_TXE)) { } // Czekaj na opróżnienie bufora
while (!(USART2->ISR & USART_ISR_TC)) { } // Czekaj na zakończenie transmisji
while(1)
{
}
}However, when I try to configure other peripherals (for example TIM2, TIM4, or GPIOs on a different port), they do not seem to initialize properly.
When stepping through the debugger, it looks like the code just skips the configuration functions — no registers are updated, no changes take effect.
All peripherals (TIM2, TIM3, TIM4, UART2) are connected to the same APB1 bus.
Summary of symptoms:
TIM3 works correctly in PWM mode and on 3 channels.
UART works correctly.
TIM2, TIM4 configuration fails — registers stay default after supposed initialization.
GPIOs on ports other than A also cannot be configured — the debugger simply skips the initialization code.
I'm wondering if this could be a clock enable issue (RCC settings?) or something else.
But when I configure 3 channels for TIM3, I have to configure also GPIO output for portB and it configures. So I assume it can be, work because off brought clock signal.
Any help would be appreciated!
Solved! Go to Solution.
2025-04-27 5:34 PM
It's probably stuck in the first timer interrupt. You enable UIE but don't check for or clear UIF in the IRQ handler, so it enters it repeatedly. Either don't set UIE or check for and clear UIF in the interrupt.
Don't read-modify write to clear flags, just write the flag you want to clear to 0.
TIM3->SR = ~TIM_SR_CC1IF; // clear CC1IF only
TIM3->SR = ~TIM_SR_UIF; // clear UIF only
2025-04-27 5:34 PM
It's probably stuck in the first timer interrupt. You enable UIE but don't check for or clear UIF in the IRQ handler, so it enters it repeatedly. Either don't set UIE or check for and clear UIF in the interrupt.
Don't read-modify write to clear flags, just write the flag you want to clear to 0.
TIM3->SR = ~TIM_SR_CC1IF; // clear CC1IF only
TIM3->SR = ~TIM_SR_UIF; // clear UIF only
2025-04-27 9:37 PM
Besides what @TDK wrote above, if running at higher frequencies, you need to set FLASH waitstates.
JW
2025-05-01 7:35 AM
@TDK You are right thanks for help. Everything works fine.
2025-05-01 7:36 AM
@waclawek.jan Thanks for advice. I set it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.