2021-08-04 3:26 PM
Hi
Using CubeMX on a STM32H7B3I I have generated this initialisation function for the TIM12 CH2
/**
* @brief TIM12 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM12_Init(void)
{
/* USER CODE BEGIN TIM12_Init 0 */
/* USER CODE END TIM12_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM12_Init 1 */
/* USER CODE END TIM12_Init 1 */
htim12.Instance = TIM12;
htim12.Init.Prescaler = 27;
htim12.Init.CounterMode = TIM_COUNTERMODE_UP;
htim12.Init.Period = 1023;
htim12.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim12.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim12) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim12, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim12) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim12, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM12_Init 2 */
/* USER CODE END TIM12_Init 2 */
HAL_TIM_MspPostInit(&htim12);
}
Then this is called as:
MX_TIM12_Init();
HAL_TIM_PWM_Start(&htim12, TIM_CHANNEL_2);
But I don't see any PWM coming out.
Could someone point out what could be wrong?
thanks
2021-08-04 5:14 PM
> sConfigOC.Pulse = 0;
You have set up a 100% duty cycle PWM, which is a DC signal.
Change this to something between 0 and the Period value to get a square wave.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.