2012-09-10 12:25 AM
In my application I set up SysTick with:
SysTick_Config(SystemCoreClock / 1000);to generate a 1ms interrupt.I got some weird timing anomalies and eventually used a timer interrupt to generate 1ms interrupts using the PSC (prescale) and ARR (auto-reload) registers.When I compare the two I get about 1012 to 1032 SysTick interrupts for every 1000 timer interrupts - yup that's right folks, it varies every cycle. When I compare timer interrupts to other timer interrupts, they all report as being perfectly in sync with each other.To me, it seems that SysTick counts ''ticks'' and expecting anything more than that might not be correct. The difference probably wouldn't matter if I wasn't using a 3ppm oscillator to clock the system. Although to be honest I have no way of telling which time reference is correct.Any ideas as to what's going on?2012-09-10 6:46 PM
Okay, more details:
voidTestLoop(
void
)
{
RTC_TimeTypeDef
time
;
u16 sec = 0;
u16 tick;
u32 lastms, ms;
for
(;;)
{
RTC_GetTime(RTC_Format_BIN, &
time
);
if
(sec !=
time
.RTC_Seconds)
{
sec =
time
.RTC_Seconds;
tick = IRQ3;
IRQ3 = 0;
ms = MilliSeconds;
printf
(
''Test: %d %d %d
''
, Ticks, tick, ms - lastms);
lastms = ms;
}
}
}
Ticks is updated by a 1000Hz timer interrupt routine and counts from 0 to 9
IRQ3 is updated by a 6000Hz timer.
Milliseconds is updated by SysTick interrupt which is set as per the previous message. The RTC clock is clocked using a 32768Hz crystal on the LSE processor pins.
The output of this loop is:
Test: 345 6000 1014
Test: 345 6000 1024
Test: 345 6000 1017
Test: 345 6000 1015
Test: 345 6000 1023
Test: 345 6000 1019
Test: 345 6000 1016
Test: 345 6000 1019
Test: 345 6000 1025
Test: 345 6000 1018
Test: 345 6000 1015
Test: 345 6000 1020 after 45 minutes:
Test: 336 6000 1020
Test: 336 6000 1015
Test: 336 6000 1025
Test: 336 6000 1015
Test: 336 6000 1014 So there's 9ms of drift in 45 minutes which is 3.3ppm -or- about 0.3s of relative drift per day between the LSE and HSE clock sources.
The one that really sticks out is the variation in the SysTick number which seems to be wrong by about 20000ppm!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.