2017-10-23 3:52 AM
Hi All,
Due to CPU package change, I tried to change the CPU from Keil configuration. But the project does not work. So when I check the problem part, it is SystemClock_Config() where I am configuring the sysclk.
STM32f769NI based project is not working while stm32f769BI based project is working without any issue. I have not changed anything but the CPU.
To experiment a bit, I changed the PLL_M and PLL_N to a different value but generate same sysclk then the project works but only half the speed(Ex: 500msec timer runs 1 sec interval).
here below my SystemClock_Config function.
/**
* @brief System Clock Configuration * The system Clock is configured as follow : * System Clock source = PLL (HSE) * SYSCLK(Hz) = 200000000 * HCLK(Hz) = 200000000 * AHB Prescaler = 1 * APB1 Prescaler = 4 * APB2 Prescaler = 2 * HSE Frequency(Hz) = 8000000 * PLL_M = 4 * PLL_N = 200 * PLL_P = 2 * PLL_Q = 2 * VDD(V) = 3.3 * Main regulator output voltage = Scale1 mode * Flash Latency(WS) = 6 * @param None * @retval None */static void SystemClock_Config(void){ RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_OscInitTypeDef RCC_OscInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/* Enable HSE Oscillator and activate PLL with HSE as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.HSIState = RCC_HSI_OFF; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 200; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 2; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); }/* activate the OverDrive to reach the 200 Mhz Frequency */
if(HAL_PWREx_EnableOverDrive() != HAL_OK) { Error_Handler(); } /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_6) != HAL_OK) { Error_Handler(); } /* Select PLLSAIP as USB clock source 48MHz =((HSE/PLLM)*PLLSAIN)/PLLSAIP. Set LTDC clock to 12MHz = (((HSE/PLLM)*PLLSAIN)/PLLSAIP)/PLLSAIDivR. Select CLK48 as SDMMC1 as clock source. */ PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC|RCC_PERIPHCLK_SDMMC1|RCC_PERIPHCLK_CLK48 | RCC_PERIPHCLK_UART7; PeriphClkInitStruct.PLLSAI.PLLSAIN = 96; PeriphClkInitStruct.PLLSAI.PLLSAIR = 4; PeriphClkInitStruct.PLLSAI.PLLSAIQ = 2; PeriphClkInitStruct.PLLSAI.PLLSAIP = RCC_PLLSAIP_DIV4; PeriphClkInitStruct.PLLSAIDivQ = 1; PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_4; PeriphClkInitStruct.Clk48ClockSelection = RCC_CLK48SOURCE_PLLSAIP; PeriphClkInitStruct.Sdmmc1ClockSelection = RCC_SDMMC1CLKSOURCE_CLK48; PeriphClkInitStruct.Uart7ClockSelection = RCC_UART7CLKSOURCE_PCLK1; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { Error_Handler(); }}Sorry if anything wrong in my post since it is my first one.
2017-10-25 7:19 PM
Any insights please?
2017-10-25 10:40 PM
Does it 'work' if you use the HSI as the clock source?
Have you exported internal clocks via the PA8 (MCO) pin?
Does it get stuck in the Error_Handler()
Have you compared any of the RCC or peripheral registers between the two designs?
2017-10-30 7:42 PM
Sorry for the late reply.
To make it simpler, I copied an RTX blink program with 25MHZ clock. Since my hardware is 8MHZ, I just reconfigured that portion.
When I tried to configure the CCR to achieve HCLK = 200MHZ, It always goes to Hardfault_handler or Can not stop debugger state whether the clock source is HSI or HSE.
Using MCO2 on PC9 pin, I am able to see the PLLCLK is generating 200MHZ. with the AHB prescaller is set to 1, HCLK is supposed to be same as PLLCLK.
I compared the working CPU RCC registers and not working CPU RCC registers. It is more or less same(Same in the necessary section).
Just to try, I reduced the clock to 150MHZ by changing the PLLM and PLLN, I am able to see my LED blinking. And I am able to see the LED blinking when I comment out the OS functions with 200mhz sysclk.
And one new update is that if I enable MicroLIB option then I am able to see the LED blinking even with the OS functions. I do not have much experience with RTX hence i'm clueless about the issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.