2017-10-30 5:57 PM
Hi,
I have interfaced S34ML04G2(nand flash) with STM32F723 controller and using built-in FMC controller to read the Nand flash.
I am using 'HAL_NAND_Read_Page_8b()' to read the entire page and have hooked up a logic analyzer on the interface.
I configured the FMC timings as per AN2784 ('Using the high-density STM32F10xxx FSMC peripheral to drive external memories').
When I read the entire page, I see a huge delay between each byte read (220 - 150ns) {see attached scope capture - &sharpCE1 goes high between each data access}. This is a huge delay in 5ns world (My HCLK is 200MHz).
Essentially the code being executed during the scope capture is:
/* Get Data into Buffer */
for(; index < size; index++){*(uint8_t *)pBuffer++ = *(uint8_t *)deviceAddress;}My timing settings are:
/* hnand1.Init */
hnand1.Init.NandBank = FMC_NAND_BANK3;hnand1.Init.Waitfeature = FMC_NAND_WAIT_FEATURE_ENABLE;hnand1.Init.MemoryDataWidth = FMC_NAND_MEM_BUS_WIDTH_8;hnand1.Init.EccComputation = FMC_NAND_ECC_DISABLE;hnand1.Init.ECCPageSize = FMC_NAND_ECC_PAGE_SIZE_2048BYTE;hnand1.Init.TCLRSetupTime = 0;hnand1.Init.TARSetupTime = 0;/* hnand1.Config */hnand1.Config.PageSize = 2048;hnand1.Config.SpareAreaSize = 128;hnand1.Config.BlockSize = 64;hnand1.Config.BlockNbr = 8192;hnand1.Config.PlaneNbr = 2;hnand1.Config.PlaneSize = 4096;hnand1.Config.ExtraCommandEnable = DISABLE;/* ComSpaceTiming */ComSpaceTiming.SetupTime = 1;ComSpaceTiming.WaitSetupTime = 3;ComSpaceTiming.HoldSetupTime = 2;ComSpaceTiming.HiZSetupTime = 1;Anyone, who has a hint on who would have caused this delay? Apparently, this is bare metal code, so no clock cycles are lost during execution.
I have enabled the ART and I-cache (when I enable the D-cache, I see a different problem, which I can also discuss if anyone is willing to look )
Any help would be greatly appreciated.
Thanks,
AQ
#fmc #nand-flashWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.