2024-04-17 12:10 AM
Hello everyone
I'll receive soon a custom board based on an STM32 microcontroller (still not sure about the specific part number) and I'll have to flash FW updates on it. A few questions about it:
1) There's a 4 pin header connector on the board (VCC, SWCLK, GND, SWO) and I have two STLink programmers (STLink V2 and V2/ISOL). Is this connection scheme correct? (Left header connector, right STLink 20 pin connector).
VCC -> 1
SWCLK -> 9
GND -> 3
SWO -> 13
2) Will this work fine even if I have no SWDIO pin on the header connector?
Thank you very much in advanced
Nick
Solved! Go to Solution.
2024-04-17 12:45 AM - edited 2024-04-17 12:51 AM
@NDicostanzo wrote:2) Will this work fine even if I have no SWDIO pin on the header connector?
No: you need SWDIO for programming!
It would also be wise to provide NRST on the programming connector - this can get you out of some "stuck" situations.
https://wiki.segger.com/Target_Interface_SWD
https://developer.arm.com/documentation/101636/0100/Debug-and-Trace/JTAG-SWD-Interface
#SWD #SWDConnector
2024-04-17 12:45 AM - edited 2024-04-17 12:51 AM
@NDicostanzo wrote:2) Will this work fine even if I have no SWDIO pin on the header connector?
No: you need SWDIO for programming!
It would also be wise to provide NRST on the programming connector - this can get you out of some "stuck" situations.
https://wiki.segger.com/Target_Interface_SWD
https://developer.arm.com/documentation/101636/0100/Debug-and-Trace/JTAG-SWD-Interface
#SWD #SWDConnector
2024-04-17 12:55 AM
Thank you very much. This confirms my initial concerns.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.