2018-02-12 7:27 PM
Posted on February 13, 2018 at 04:27
Boards: STM32F0 Discovery, STM32F4 Discovery
OS: Windows 8.1 x64
GUI: PlatformIO
Tried the following multiple times with restarts, uninstalls:
PlatformIO cannot build on device. I gave it to my friend and he was able to flash both disco boards no problem in Linux.
Forum links:
[UPDATE] I used the driver from
and both boards work no problem
2018-02-14 1:11 PM
@Community member
thanks for the update, now you are using the right driver for ST-Link HW, The VCP driver one is used for our USB devices example called VCP generated by CubeMX or in our HAL examples.
Cheers,
STOne-32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.