2018-02-14 7:59 AM
Hello. I'm driving The RTC On STM32F4 Discovery and I'm using STM32Cube for initialization. after everything, It only updates the value after a Reset. I don't know what the problem is. Can you help?
Here is the code for my main.c :
int main(void)
{ /* USER CODE BEGIN 1 *//* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_I2C1_Init(); MX_I2S3_Init(); MX_SPI1_Init(); MX_USB_HOST_Init(); MX_RTC_Init(); /* USER CODE BEGIN 2 */ RTC_TimeTypeDef stime; /* USER CODE END 2 *//* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) {/* USER CODE END WHILE */
MX_USB_HOST_Process();/* USER CODE BEGIN 3 */
MX_RTC_Init(); HAL_RTC_GetTime(&hrtc, &stime, FORMAT_BIN); printf('second : %d, minute : %d, hour : %d\n', stime.Seconds, stime.Minutes, stime.Hours); HAL_Delay(100); } /* USER CODE END 3 */}
and here the code that Cube generated:
void MX_RTC_Init(void)
{ RTC_TimeTypeDef sTime; RTC_DateTypeDef sDate;/**Initialize RTC Only
*/ hrtc.Instance = RTC;if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0x32F2){ hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 100-1; hrtc.Init.SynchPrediv = 320-1; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; if (HAL_RTC_Init(&hrtc) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Initialize RTC and set the Time and Date
*/ sTime.Hours = 0x17; sTime.Minutes = 0x0; sTime.Seconds = 0x0; sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; sTime.StoreOperation = RTC_STOREOPERATION_RESET; if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }sDate.WeekDay = RTC_WEEKDAY_WEDNESDAY;
sDate.Month = RTC_MONTH_FEBRUARY; sDate.Date = 0x14; sDate.Year = 0x18;if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,0x32F2);
}}
void HAL_RTC_MspInit(RTC_HandleTypeDef* rtcHandle)
{if(rtcHandle->Instance==RTC)
{ /* USER CODE BEGIN RTC_MspInit 0 *//* USER CODE END RTC_MspInit 0 */
/* RTC clock enable */ __HAL_RCC_RTC_ENABLE(); /* USER CODE BEGIN RTC_MspInit 1 *//* USER CODE END RTC_MspInit 1 */
}}void HAL_RTC_MspDeInit(RTC_HandleTypeDef* rtcHandle)
{if(rtcHandle->Instance==RTC)
{ /* USER CODE BEGIN RTC_MspDeInit 0 *//* USER CODE END RTC_MspDeInit 0 */
/* Peripheral clock disable */ __HAL_RCC_RTC_DISABLE(); /* USER CODE BEGIN RTC_MspDeInit 1 *//* USER CODE END RTC_MspDeInit 1 */
}}what is it here that i'm doing wrong?
2018-02-14 10:17 AM
Read the reference manual for your particular part. You need to fetch both time AND date in order to read the values from the shadow registers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.