2011-08-22 2:51 AM
Hi:
Hello, everyone, I want to ask a question about STM32W108 I according tothe official schematics for the design (in some places has been modified).STM32W108 chip pin is 40, but with RF4CE firmware library, but to which the programming procedure, into an assertion that the program is always a function, and ultimately into an infinite loop, I do not know why. Errors appear here: halInit ()----> halPowerUp ();----> halInternalInitAdc (); ----> stCalibrateVref (); ----> halCommonGetMfgToken (& biasTrim, TOKEN_MFG_ANALOG_TRIM_BOTH);, to here the next sentence assertionfunction: if (biasTrim.auxadc == 0xFFFF) {assert (FALSE);} will loop on the inside, and I do not know typedef struct { int16u iffilterH; int16u biasmaster; int16u moddac; int16u auxadc; int16u caladc;} TokTypeMfgAnalogueTrimBoth;I do not know where the error causes this result, and who can help me? Thank you! #stm32w1082011-08-22 4:07 PM
It's asserting because you have a bogus value in the structure. An assert() is there to check and catch stupid settings, the assert triggers because it found one.
You need to work backwards from where it's asserting, and find where it's initializing the structure, and writing values in to it. Try searching on ''auxadc ='' for instance would be a pretty basic step.2011-08-22 7:17 PM
When I
single-step
simulation
,
to
this sentence
: stCalibrateVref ();,
pop up
a
dialog box
,
shown above
do not
find some
files
,
such as
transmission.c,
I
find the
installation
directory
, but no
transmission.c
file
I
would like to ask
,
this
file
will
affect
my program
it?
If it does,can
you
send me a
transmission.c
file?
Thank you
!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.