2021-11-11 11:53 AM
I'm evaluating the STM32U585 TLS performance using the eval board B-U585I-IOT02A. The example application code for MQTT using TLS did not include code on how to load a client key for client authentication but I was able to add that in. The problem I see now is that when using private key the MCU takes 13 seconds to do the RSA computations during the handshake with the server to setup the connection. I track the delay to the following function _nx_crypto_huge_number_mont_power_modulus
Why does this take so long? Does the MCU have hardware acceleration that handles this and is just not being used? Is there something else that I'm doing wrong?
2021-12-03 9:29 AM
Hello @RCost.1
yes the STM32U5 version used in the B-U585I-IOT02A embeds a Public Key Accelerator. The implementation of the connection to this accelerator is ongoing and should be available on next release.
Best regards
Jocelyn
2021-12-03 11:56 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.