2022-06-24 5:40 AM
Hi,
I would like to test OTFDEC on STM32U585 to use it inside a custom BOOTLOADER.
For my test, I use online website to compute AES CTR on this plaintext data "azertyuioqsdfghj" with the key 0x01020304050607081112131421222324 (I discuss IV further).
I set the data directly in source code and run my application. It write the data in HyperFlash at address 0x70001000. In addition, the I use OTFDEC to display decrypt value.
My issue is that I cannot recover the plaintext Data.
What is the IV for OTFDEC (I set NONCE and version to 0)?
I think I have an issue with IV but I am not sure.
Can someone give me an example with an external tool to create cryptic data?
Can someone explain me how OTFDEC works?
What is the IV really used If I configure OTFDEC to start at 0x70001000 address (with nonce and version set to 0)?
Thanks a lot for helping me.
Have a good day.
Aurélien
2022-07-22 2:41 AM
Hello @Aurelien and welcome to the community,
What do you mean by IV for OTFDEC?
You can have a look on this application note to learn more about the OTFDEC
You can follow the OTFDEC configuration from this example from the STM32U5 Firmware
Project path: "STM32Cube_FW_U5_V1.1.0\Projects\B-U585I-IOT02A\Examples\OTFDEC\OTFDEC_Data_Decrypt"
Mohamed Aymen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.