2025-03-11 6:47 AM
Hi,
Does anyone know if there is a chance for a new N6-device later this year having built in flash of at least 4MB?
Our project is currently based on a one chip solution with a custom U5-board with built in FLASH/RAM of 4MB and a 5” Riverdi display. However, we need to migrate to a 7” Riverdi display and a MCU with higher performance. We are in strong favour of shorten time-to-market by keeping a low complexity integration (i.e. no external memories) and a straightforward PCB design.
It would be really helpful to us if any plausible market intentions from ST are given.
Thanks in advance
Solved! Go to Solution.
2025-03-11 7:03 AM
Hello,
STM32N6 product is intended to be Flashless. I don't think there will be a version with an embedded flash at least in the near future (1 year).
2025-03-11 7:03 AM
Hello,
STM32N6 product is intended to be Flashless. I don't think there will be a version with an embedded flash at least in the near future (1 year).
2025-03-12 8:47 AM
Thanks for your reply.
However that was disappointing to hear.
From a business point of view, I think such a product could be disruptive and offer an interesting market opportunity for ST.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.