2026-03-17 9:37 AM
I was wondering if there is any possibility to change the NCS from NCS1_port2 to NCS2_port2 using the OTP registers on the STM32N6.
I checked the registers but couldn’t find any option to adjust this. Maybe its not possible.
Just to confirm my understanding:
The default setting for ROM boot is XSPI1 using XSPIM_Port_2, and NCS1 is "required" by the ROM boot code to correctly load the FSBL via LoadAndRun.
Kind regards,
Zimmeri
Solved! Go to Solution.
2026-04-01 4:39 AM
Hello!
I was wondering if there is any possibility to change the NCS from NCS1_port2 to NCS2_port2 using the OTP
registers on the STM32N6.
=> It is not possible, there is no OTP registers doing that. The NCS used by the ROM boot is fixed
The default setting for ROM boot is XSPI1 using XSPIM_Port_2, and NCS1 is "required" by the ROM boot code to correctly load the FSBL via LoadAndRun
=>Yes
Best regards
ANJS
2026-04-01 4:39 AM
Hello!
I was wondering if there is any possibility to change the NCS from NCS1_port2 to NCS2_port2 using the OTP
registers on the STM32N6.
=> It is not possible, there is no OTP registers doing that. The NCS used by the ROM boot is fixed
The default setting for ROM boot is XSPI1 using XSPIM_Port_2, and NCS1 is "required" by the ROM boot code to correctly load the FSBL via LoadAndRun
=>Yes
Best regards
ANJS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.