2021-05-26 4:54 AM
1. It is correct to read and write flash through command function when there is no memory mapping enabled( flash:MX25R6435F )
2. After memory mapping is enabled, after accessing the address of 0x90000000, the MCU crashes and cannot recognize the chip. I suspect that there is a problem with the configuration memory mapping?? Please help me!!!
-----------------------------------------------------------------------------------------------------------------------------------
//Enable memory mapping
uint8_t BSP_OSPI_NOR_EnableMemoryMappedMode(void)
{
OSPI_RegularCmdTypeDef s_command;
OSPI_MemoryMappedTypeDef s_mem_mapped_cfg = {0};
/* Initialize the read command */
if (OSPI_NOR_WriteEnable(&hospi1) != HAL_OK)
{
return HAL_ERROR;
}
s_command.OperationType = HAL_OSPI_OPTYPE_READ_CFG;
s_command.FlashId = HAL_OSPI_FLASH_ID_1;
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
s_command.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
s_command.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
s_command.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = HAL_OSPI_DATA_4_LINES;
s_command.DummyCycles = 8;
s_command.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
s_command.Instruction = MX25R6435F_FLASH_CMD_FAST_READ;//MX25R6435F_FLASH_CMD_4READ;
s_command.Address = 0;
s_command.NbData = 1;
s_command.DQSMode = HAL_OSPI_DQS_DISABLE;
/* Send the read command */
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
mprintf("BSP_OSPI_NOR_Read %d",__LINE__);
return HAL_ERROR;
}
s_command.OperationType = HAL_OSPI_OPTYPE_WRITE_CFG;
s_command.Instruction = MX25R6435F_FLASH_CMD_4PP;
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
s_command.AddressMode = HAL_OSPI_ADDRESS_4_LINES;
s_command.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
s_command.DataMode = HAL_OSPI_DATA_4_LINES;
s_command.DummyCycles = 0;
s_command.DQSMode = HAL_OSPI_DQS_ENABLE;
/* Send the write command */
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
mprintf("BSP_OSPI_NOR_Read %d",__LINE__);
return HAL_ERROR;
}
/* Configure the memory mapped mode */
s_mem_mapped_cfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
if (HAL_OSPI_MemoryMapped(&hospi1, &s_mem_mapped_cfg) != HAL_OK)
{
mprintf("BSP_OSPI_NOR_Read %d",__LINE__);
return HAL_ERROR;
}
//uint8_t * psram = (uint8_t *)0x90000000;
//mprintf("psram[0]=%d [1]=%d [2]=%d [3]=%d",psram[0],psram[1],psram[2],psram[3]);
return HAL_OK;
}
Solved! Go to Solution.
2021-05-26 6:26 AM
1) You should do the read/write/erase operations in command mode. An equivalent read command that works properly in command mode should also be viable when you switch into memory-mapped mode.
2) What exactly is happening? It Hard Faults?
Unfortunately the provided code lacks a lot of detail/context to determine what it wrong.
2021-05-26 6:26 AM
1) You should do the read/write/erase operations in command mode. An equivalent read command that works properly in command mode should also be viable when you switch into memory-mapped mode.
2) What exactly is happening? It Hard Faults?
Unfortunately the provided code lacks a lot of detail/context to determine what it wrong.
2021-05-27 6:57 PM
Thank you. I have settled it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.