2019-06-03 6:35 AM
I have to read out a Mems-Mic (SPH0645LM4H-B).
The Data Format is I2S, 24-bit, 2’s compliment, MSB first.
One Cannel (L/R) needs 32 clocks -> Framlenght = 64
Samplerate 48kHz, real 46,875kHz, Clock 3.072MHZ.
Seems OK.
BUT: the FS-Signal Duty_Cycle is wrong!
Should be 1:1
In the Attachment you can see my SAI1_Init-Settings.
Whats wrong ?
Or to do to get a correct FS_Signal?
Kind Regards
Runout
2019-06-03 7:42 AM
Read out and check the SAI registers content. You probably want to concentrate on SAI_xFRCR.FSALL, look it up in the Reference Manual. I don't understand the Cube gibberish, but maybe it's related to ActiveFrameLength in the init struct.
JW
2019-06-04 1:04 AM
Hi Jan,
thank for your advice.
hsai_BlockA1.FrameInit.FrameLength = 64;
hsai_BlockA1.FrameInit.ActiveFrameLength = 32;
is correct.
To HAL o nor to HAL...
The "wording" is horrible.
Differs between CubeMx, HAL_Driver and MCU-Register.
Kind Regards Thomas
(maybe there are further questions...)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.