2018-04-08 12:13 AM
L496 port G includes two I2C- PG13/14 I2C1 and PG7/8 I2C3. But the two I2C cannot output and the oscilloscope does not display waveform.
I2C1/I2C3 can work correctly if they are mapped to other ports. So I think the I2C1/I2C3 modules are ok in L496.
On the other hand, if I set PG13/14 and PG7/8 pin mode as GPIO output, they can work well. So the GPIOG module is ok.So what is the problem with GPIOG I2C? I know Port G[15:2] are independent from other ports. But I connect Vddio2 to Vdd in the test. Please see the code below.
Init Code:
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOG); HAL_PWREx_EnableVddIO2();LL_GPIO_SetPinMode(GPIOG, LL_GPIO_PIN_13, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetAFPin_0_7(GPIOG, LL_GPIO_PIN_13, LL_GPIO_AF_4); LL_GPIO_SetPinSpeed(GPIOG, LL_GPIO_PIN_13, LL_GPIO_SPEED_FREQ_HIGH); LL_GPIO_SetPinOutputType(GPIOG, LL_GPIO_PIN_13, LL_GPIO_OUTPUT_OPENDRAIN); LL_GPIO_SetPinPull(GPIOG, LL_GPIO_PIN_13, LL_GPIO_PULL_UP); LL_GPIO_SetPinMode(GPIOG, LL_GPIO_PIN_14, LL_GPIO_MODE_ALTERNATE); LL_GPIO_SetAFPin_0_7(GPIOG, LL_GPIO_PIN_14, LL_GPIO_AF_4); LL_GPIO_SetPinSpeed(GPIOG, LL_GPIO_PIN_14, LL_GPIO_SPEED_FREQ_HIGH); LL_GPIO_SetPinOutputType(GPIOG, LL_GPIO_PIN_14, LL_GPIO_OUTPUT_OPENDRAIN); LL_GPIO_SetPinPull(GPIOG, LL_GPIO_PIN_14, LL_GPIO_PULL_UP);Read Code:
LL_I2C_Enable(I2C1); LL_I2C_HandleTransfer(I2C1, add, LL_I2C_ADDRSLAVE_7BIT, 2, LL_I2C_MODE_AUTOEND, LL_I2C_GENERATE_START_READ); while (!LL_I2C_IsActiveFlag_STOP(I2C1)) { if (LL_I2C_IsActiveFlag_RXNE(I2C1)) { i2c1Ctx.rxBuffer[0] = LL_I2C_ReceiveData8(I2C1); } } LL_I2C_ClearFlag_STOP(I2C1);Solved! Go to Solution.
2018-06-06 6:32 AM
If you are setting a GPIO pin greater than 7 to an alternate function, you need to use the LL_GPIO_SetAFPin_8_15 function. eg.
LL_GPIO_SetAFPin_8_15(GPIOG,
LL_GPIO_PIN_13
, LL_GPIO_AF_4);2018-04-08 7:41 AM
Make sure the PWR peripheral's clock is enabled
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
You want code equivalent to
/* VddIO2 must be enabled to access GPIO port G[2:15] */
__HAL_RCC_PWR_CLK_ENABLE(); HAL_PWREx_EnableVddIO2(); __HAL_RCC_GPIOG_CLK_ENABLE();2018-04-12 5:27 AM
Thanks Clive. I use HAL driver and it can work now. It would be some I2C setting problems in LL library.
Actually I don't want to use HAL because it's too big and inefficient. Thanks your help again.
2018-04-12 10:33 AM
Hi
Mei.Raymond
,Could you please explain how you did resolved the issue with pins in port G to be used with I2C?
Thanks.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-04-12 5:57 PM
I just used the demo in your Nucleo package,
STM32Cube_FW_L4_V1.10.0\Projects\STM32L496ZG-Nucleo\Examples\I2C\I2C_TwoBoards_ComPolling
I have not compared the detail difference in HAL and LL library for I2C setting. I think it is a bug to config Port G I2C1/3 in LL. Hope ST can fix it in the future. Thanks.
2018-06-06 6:32 AM
If you are setting a GPIO pin greater than 7 to an alternate function, you need to use the LL_GPIO_SetAFPin_8_15 function. eg.
LL_GPIO_SetAFPin_8_15(GPIOG,
LL_GPIO_PIN_13
, LL_GPIO_AF_4);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.