2018-06-05 8:23 AM
ST seems to do reading all files in a directory in a hard way.
I am combining two examples about Sdfat but ST uses unfamiliar commands for reading all files in a directory. I think I could do it with a hard way but isn't f_findfirst/f_findnext more common.
I have examples for reading all bmp files and an other showing one jpg file.
Edit: By the way. I still have to accept cookies several times in one session.
Solved! Go to Solution.
2018-06-05 4:03 PM
In ffconf.h
♯ define _USE_FIND 1
/* This option switches filtered directory read functions, f_findfirst() and/ f_findnext(). (0:Disable, 1:Enable 2:Enable with matching altname[] too) */They compile a short list, in much the same way as you might populate the entries in a COMBO_BOX, in much the same way I'd display a list of Firmware .BIN files and ask the user to pick one, then I can load the selected one immediately rather than enumerate the files. The latter being problematic in a multi-tasking system where new files could appear, or old ones get deleted, and the indexes would change.
2018-06-05 8:47 AM
>>Any examples with f_findfirst/f_findnext for 746D?
Why make this F746 or STM32 specific, FatFS is platform agnostic.
Is there an issue with this example?
http://elm-chan.org/fsw/ff/doc/findfirst.html
>>ST uses unfamiliar commands for reading all files in a directory.
Ok, but what does that mean, unfamiliar to them, to you, others practiced in the art?
STM32Cube_FW_F7_V1.11.0\Projects\STM32746G-Discovery\Applications\Display\LTDC_PicturesFromSDCard\Src\fatfs_storage.c
/**
* @brief List up to 25 file on the root directory with extension .BMP * @param None * @retval The number of the found files */uint32_t Storage_GetDirectoryBitmapFiles (const char* DirName, char* Files[]){ FRESULT res; uint32_t index = 0;/* Open filesystem */
if(f_mount(&fs, (TCHAR const*)'',0) != FR_OK) { return 0; }/* Start to search for wave files */
res = f_findfirst(&dir, &fno, DirName, '*.bmp');/* Repeat while an item is found */
while (fno.fname[0]) { if(res == FR_OK) { if(index < MAX_BMP_FILES) { sprintf (Files[index++], '%s', fno.fname); } /* Search for next item */ res = f_findnext(&dir, &fno); } else { index = 0; break; } }f_closedir(&dir);
return index;
}>>By the way. I still have to accept cookies several times in one session.
Some settings or plug-ins at your end, this isn't an issue for 99.99% of users here. If it becomes sufficiently annoying, then change your behaviour.
2018-06-05 3:41 PM
My C or Sdfat skills are in no way perfect. I get this error just inserting the function
'STM32746G-DISCOVERY\Exe\Project.axf: Error: L6218E: Undefined symbol f_findfirst (referred from main.o).' and same from findnext. I use STM32Cube_FW_F7_V1.11.0\Projects\STM32746G-Discovery\Applications\LibJPEG as basis, it uses Sdfat but clearly something is missing.
>>ST uses unfamiliar commands for reading all files in a directory.
'Ok, but what does that mean, unfamiliar to them, to you, others practiced in the art?'
I wonder what is the reason not using f_findnext. I have probably used them elsewhere and it was easy enough I think. Having an array to store file names eats ram.
2018-06-05 3:48 PM
Hello
Michael.Lei
,follow FatFS docs and you will see how to enable f_findfirst/next functions:
http://elm-chan.org/fsw/ff/doc/findfirst.html
Best regard,Tilen
2018-06-05 4:03 PM
In ffconf.h
♯ define _USE_FIND 1
/* This option switches filtered directory read functions, f_findfirst() and/ f_findnext(). (0:Disable, 1:Enable 2:Enable with matching altname[] too) */They compile a short list, in much the same way as you might populate the entries in a COMBO_BOX, in much the same way I'd display a list of Firmware .BIN files and ask the user to pick one, then I can load the selected one immediately rather than enumerate the files. The latter being problematic in a multi-tasking system where new files could appear, or old ones get deleted, and the indexes would change.
2018-06-05 4:14 PM
I added #include 'ffconf.h' but still get the same undefined error. I wonder if this is some Keil 'feature' here you have to tell paths elsewhere too, but Sdfat is already working so I wonder.
I found
http://elm-chan.org/fsw/ff/doc/findfirst.html
after same searching and it is quite good information. But something is missing, includes or something or some other setting. Because I allways get errors.This is the beginning of the main.c
/* Includes ------------------------------------------------------------------*/#include 'main.h'#include 'ffconf.h'/* Private typedef -----------------------------------------------------------*//* Private define ------------------------------------------------------------*/#include 'ff.h'/* Private macro -------------------------------------------------------------*//* Private variables ---------------------------------------------------------*/FATFS SDFatFs; /* File system object for SD card logical drive */FIL MyFile; /* File object */FRESULT res;DIR dir;static FILINFO fno;//char* pDirectoryFiles[MAX_BMP_FILES];char* pDirectoryFiles[30];uint8_t ubNumberOfFiles = 0;uint32_t uwBmplen = 0;char SDPath[4]; /* SD card logical drive path */RGB_typedef *RGB_matrix;uint8_t _aucLine[2048];uint32_t offset = 0;uint32_t line_counter = 239;/* Private function prototypes -----------------------------------------------*/static void SystemClock_Config(void);static void LCD_Config(void);static uint8_t Jpeg_CallbackFunction(uint8_t* Row, uint32_t DataLength);static void CPU_CACHE_Enable(void);/* Private functions ---------------------------------------------------------*//* Search a directory for objects and display it */�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�? .
2018-06-05 4:15 PM
The code combiled without errors. That
'In ffconf.h
#define _USE_FIND 1->0 helped. But I don't want edit shared include files. I have to do some testing still, copy the file in my main.c folder probably. It is also getting late here,I'll continue tomorrow.
I thank you Clive and Tilen. This is much better now.
Edit: ffconf.h is project specific in this project, no need to fear about messing other projects
2018-06-05 4:16 PM
I answered but included some code we'll see. But in short &sharpinclude 'ffconf.h' did not help
2018-06-05 4:45 PM
ff.c needs to build against ffconf.h settings..
2018-06-05 6:04 PM
'In ffconf.h
&sharpdefine _USE_FIND 1
/* This option switches filtered directory read functions, f_findfirst() and/ f_findnext(). (0:Disable, 1:Enable 2:Enable with matching altname[] too) */'There is
no
&sharpdefine _USE_FIND 1 inffconf.h
from\STM32Cube\Repository\STM32Cube_FW_F7_V1.11.0\Projects\STM32746G-Discovery\Applications\DisplayLTDC_PicturesFromSDCard\MDK-ARM
or
STM32Cube\Repository\STM32Cube_FW_F7_V1.11.0\Projects\STM32746G-Discovery\Applications\LibJPEGLibJPEG_Decoding\MDK-ARM
There is not &sharpdefine _USE_FIND 1 text because it is 0. My mistake. I have to change it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.