2021-06-14 12:31 AM
Hi all,
I have a function that prints out on a prompt the current RTC Date and Time values from the RTC module... basicaly when it's called it goes like this:
RTC_TimeTypeDef rmi_time = {0};
RTC_DateTypeDef rmi_date = {0};
HAL_RTC_GetTime(&hrtc, &rmi_time, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &rmi_date, RTC_FORMAT_BIN);
service_msg_out.config.rtclock.year = rmi_date.Year;
service_msg_out.config.rtclock.month = rmi_date.Month;
service_msg_out.config.rtclock.day = rmi_date.Date;
service_msg_out.config.rtclock.weekday = rmi_date.WeekDay;
service_msg_out.config.rtclock.hour = rmi_time.Hours;
service_msg_out.config.rtclock.minute = rmi_time.Minutes;
service_msg_out.config.rtclock.second = rmi_time.Seconds;
service_msg_out.config.rtclock.has_subsecond = true;
service_msg_out.config.rtclock.subsecond = rmi_time.SubSeconds;The RTC is using a 32.768 KHz oscillator, and that works from a HW perspective. The RTC init is almost the default from CubeMX (with a slight change):
void MX_RTC_Init(void)
{
RTC_TimeTypeDef sTime = {0};
RTC_TimeTypeDef alarm_Time = {0};
RTC_DateTypeDef sDate = {0};
RTC_AlarmTypeDef alrm_a = {0};
/** Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN Check_RTC_BKUP */
if(0x0D15EA5E != RTC->BKP0R)
{
init_rtc = true;
RTC->BKP0R = 0x0D15EA5E;
}
/* USER CODE BEGIN Set alarm event */
alarm_Time.Hours = 22;
alarm_Time.Minutes = 0;
alarm_Time.Seconds = 0;
alarm_Time.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
alrm_a.Alarm = RTC_ALARM_A;
alrm_a.AlarmMask = RTC_ALRMAR_MSK4;
alrm_a.AlarmTime = alarm_Time;
alrm_a.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
if (HAL_RTC_SetAlarm(&hrtc, &alrm_a, RTC_FORMAT_BIN) != HAL_OK)
{
Error_Handler();
}
__HAL_RTC_ALARMA_ENABLE(&hrtc);
__HAL_RTC_ALARM_EXTI_ENABLE_EVENT();
/** Initialize RTC and set the Time and Date
*/
if(init_rtc)
{
sTime.Hours = 0;
sTime.Minutes = 0;
sTime.Seconds = 0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
{
Error_Handler();
}
sDate.WeekDay = RTC_WEEKDAY_SATURDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 1;
sDate.Year = 0;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
{
Error_Handler();
}
init_rtc = false;
}
}But my main question is the following:
Is there any explanation for that, am I reading or configuring the RTC wrong?
Cheers,
Alberto
2021-06-14 12:40 AM
Although the code you've presented does this, do you always read out date after time?
JW
2021-06-14 3:20 AM
Hi JW, yes, I always do that in all the places, however, thanks very much for that interesting link, I'm trying the double/triple readout and it seems to be working reliably now... but early days...
equal = false;
while(false == equal)
{
HAL_RTC_GetTime(&hrtc, ¤t_time, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, ¤t_date, RTC_FORMAT_BIN);
HAL_RTC_GetTime(&hrtc, &aux_time, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &aux_date, RTC_FORMAT_BIN);
if(current_time.SubSeconds == aux_time.SubSeconds)
{
equal = true;
}
}Ideally it's something I'd avoid.... but fortunately the time readout happens seldom only.
Cheers,
Alberto
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.