2017-10-23 1:16 AM
Hello to every one,
could anyone clarify something about the capacity of every FIFO stage description?
At datasheet main features, in reception part, there is a:
'Two receive FIFO with 3 stages'
Which is the capacity of every stage? At 42.3.4 there is a description where can be read: '3 complete messages can be stored un each FIFO'.
Does it mean that one message is equivalent, exactly, to one CAN frame or is it a concrete number of bytes per FIFO stage? If it is a concrete number of bytes (so different to the number of bytes of a complete frame) I haven't found this information in any part of the datasheet.
How many bytes every FIFO stage can store? how many bytes a 'complete message' is reffered?
I would like to force an overload for testing purposes and I need to have this issue clarified.
Thanks in advance.
#stm32l4 #can-fifo #stm32l476 #can-rx #can-architecture2017-10-23 2:37 AM
Total of 6 whole frames, each payload can have up to 8 bytes, per DLC.
2017-10-23 5:11 AM
Ho Clive, thanks
hence, excuse me, if I understood your replay, you mean:
or
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.