2018-09-27 11:45 AM
I have a STM32L432KC board purchased by a colleague. I installed STLink device drivers according to sheet and try to set it up. However, it never gets recognized as a STLink device (neither on Windows 7 nor on Mac OS Majove) but rather as a J-Link device when I power it on via USB and the jumper is off. Does any idea why is it that? Production error or am I missing something ? (Note: stm directly connected to laptop without any other peripherial)
2018-09-27 1:26 PM
Segger provided a firmware to create a J-Link OB, this was likely applied.
See Chapter 3 https://www.segger.com/downloads/application-notes/AN00021
https://www.segger.com/products/debug-probes/j-link/models/other-j-links/st-link-on-board/
Use it as a J-Link, or convert back
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.