STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I can't clear RCC flag (RCC_ClearFlag in stm32f103)

Hi guys!I have a problem with stm32f103, I want to check MCU Reset cause, I use RCC_GetFlagStatus is ok, after that i'll clear rcc flag but It's not working & MCU not working when user RCC_ClearFlag. If i remove RCC_ClearFlag function then MCU work n...

TPham.10 by Associate II
  • 1219 Views
  • 1 replies
  • 0 kudos

STM32F722CV - USART1 RX Interrupt not working.

Hello, I am trying to communicate MCU with using USART1 but interrupt never triggered in MCU.First I am using some definitions. Here is definitions for USART1.#define USART1_PINS_PORT GPIOA #define USART1_RX_PIN GPIO_PIN_10 #define USART1_TX_PIN ...

�?Ars by Associate II
  • 3736 Views
  • 8 replies
  • 0 kudos

stm32l432kc dev board debug interface?

I have a STM32L432KC board purchased by a colleague. I installed STLink device drivers according to sheet and try to set it up. However, it never gets recognized as a STLink device (neither on Windows 7 nor on Mac OS Majove) but rather as a J-Link de...

OCosk by Associate
  • 1161 Views
  • 1 replies
  • 0 kudos

I2C Slave ISSUE on STM32L0

Hi everyone,I am trying to develop a Master-Slave system using two Nucleo-L053R8 boards. The first one is the master, which sends a command to the Slave board whenever the onboard button is pushed. Each time a new message is received, the slave board...

luca_dix by Associate
  • 778 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.