2018-10-26 12:22 PM - edited 2023-11-20 9:33 AM
Hello Everyone,
I am using Nucleo-32 board in my project. I am programming USART to receive 10 character data and then transmit this 10 character data back.
Problem that I am observing is that if accidentally 11 character it is suppose to display error message after that every time I enter 10 character string, my response character shift right+1. Can someone
Please find below code:
HAL_Init();
SystemClock_Config();
GPIO_Toggle();
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
__HAL_RCC_USART1_CLK_ENABLE();
UartHandle.Instance = USART1;
UartHandle.Init.BaudRate = 4800;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
//UartHandle.Init.OverSampling=UART_OVERSAMPLING_16;
//UartHandle.Init.OneBitSampling=UART_ONE_BIT_SAMPLE_DISABLE;
UartHandle.Init.Mode = UART_MODE_TX_RX ;
if(HAL_UART_DeInit(&UartHandle) != HAL_OK)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
}
if(HAL_UART_Init(&UartHandle) != HAL_OK)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
}
LTC_2873();
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_7,GPIO_PIN_SET); // Mode RS485
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_14,GPIO_PIN_RESET); // RS485 Terminator Enable
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_SET); // RS485 Driver Enable
HAL_UART_Transmit_IT( &UartHandle,&aTxBuffer[0],strlen((const char*)aTxBuffer));
HAL_Delay(1000);
while(1)
{
do
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_RESET); // RS485 Receiver Enable
HAL_Delay(20);
while(HAL_UART_Receive_IT( &UartHandle,&aRx_Buffer[0],10)!=HAL_OK);
HAL_Delay(20);
}while(rx_cplt!=1);
HAL_Delay(50);
if(rx_cplt==1)
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_SET); // RS485 Driver Enable
HAL_Delay(20);
HAL_UART_Transmit_IT( &UartHandle,&aRx_Buffer[0],10);
HAL_Delay(20);
rx_cplt=0;
}//end of if
}//end of while(1)
}
2018-10-26 7:13 PM
Fixed lengths, and sequential rx and then tx, leave very little room for recovery or resync.
I'd approach this differently. Side step HAL and do a stateful byte level management in the IRQ Handler.
2018-10-28 9:58 AM
Can you Please elaborate?
This is what I am seeing as to what is happening
When I send data more than 10 character, HAL Rx_IT rewrites Rx_Buffer[0] with 11 character (understandable)
But at the same time it increment value of my HAL pRxBuffPtr and then when I write again it uses this incremented value.
My question is if I use &Rx_Buffer[0] why it doesnot pick up address of Rx_buffer[0]?
Below is code which gives me better result but I still haven't being able to fix the problem entirely
do
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_RESET); // RS485 Receiver Enable
HAL_Delay(2);
HAL_UART_Receive_IT(&UartHandle,dummy_pointer,10);
HAL_Delay(100);
//UartHandle.pRxBuffPtr= &aRx_Buffer[0];
HAL_Delay(50);
}while(rx_cplt!=1);
UartHandle.pRxBuffPtr=dummy_pointer;
if(rx_cplt==1)
{
HAL_GPIO_WritePin(GPIOB,GPIO_PIN_4,GPIO_PIN_SET); // RS485 Driver Enable
HAL_Delay(20);
HAL_UART_Transmit_IT(&UartHandle, dummy_pointer,10);
HAL_Delay(100);
HAL_UART_Transmit_IT(&UartHandle,(uint8_t*)"\r\n",strlen((const char*)"\r\n"));
HAL_Delay(20);
rx_cplt=0;
}
I am sorry I am not inclined to used DMA, as I am not 100% sure that I will not see the same problem in DMA
Please help!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.