2016-06-22 12:11 AM
Hello,
yesterday I created a small program for STM32L152 Nucleo with CubeMX. It was running but MCO set to HSE gave only 4MHz with 75% duty cycle while I measured OSCin with 8MHz. After searching a while I found that there is a special setting for the HSE oscillator modul when using an external clock signal fed into OSCin. I found this setting prepared with defines in the HAL files and changed this line accordingly: RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; //RCC_HSE_ON; Then everything was fine. Now my question is if there is a way to use this setting in the clock configuration tab in CubeMX. Otherwise I will have to correct it again any time I create new code with CubeMX. What seems strange to me is that I found no solution to this problem in the internet. Seems no one noticed before, although both are ST products. Any help is welcome Martin2016-06-22 4:38 AM
Hi Mr_M_from_G,
I see now what you have missed. The configuration window at the left of Pinout tab contains the main configuration of the MCU peripheral that you can select/switch. For other detailed configuration , you can go to ''Configuration tab -> Peripheral bottom'' and select/ modify parameters there. -Hannibal-2016-06-23 12:01 AM
Hello all,
I found myself, it is in the pinout tab under RCC -> High Speed Clock MartinWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.