2016-06-22 12:21 AM
Hello,
I created a small program with CubeMX to test STs USB device stack. My compiler (GCC) gave me a page full of warnings because of this declaration: void USBD_GetString (uint8_t *desc, uint8_t *unicode, uint16_t *len); When called a string is passed to desc, so its type is char* which causes a warning: warning: pointer targets in passing argument 1 of 'USBD_GetString' differ in signedness [-Wpointer-sign] If I change desc to char* it's fine Now I want a solution that will keep this change when I create a new version via CubeMX, that means change the source file that CubeMX copies to my program. Where are these source files located on my computer? Any ideas? Thanks Martin.2016-06-22 4:37 AM
Hi Mr_M_from_G,
Th source files used by CubeMx for each HAL library package are located under a repository in your hard drive. Try this one: C:\Users\YourUserName\STM32Cube\Repository -Hannibal-2016-06-22 11:59 PM
Thanks Hannibal,
thats it. I changed the sources and found the changes in the newly created project files MartinWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.