2016-01-10 7:11 PM
I'm using the STM32CUBE to generate codes, HSI is used as chip's PLL clock source and the LSI is used as RTC's clock source. RTC is configured to wakeup the chip every 60 seconds.
When the chip powered up, it entered into standby mode. The next, RTC wakeup the chip, but it won't enter into standby mode again. It seems nothing is works correctly except GPIO. What should I do after it wakeup from standby mode?/* RTC init function */void MX_RTC_Init(void){ RTC_TimeTypeDef sTime; RTC_DateTypeDef sDate; /**Initialize RTC and set the Time and Date */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; HAL_RTC_Init(&hrtc); sTime.Hours = 0x0; sTime.Minutes = 0x0; sTime.Seconds = 0x0; sTime.TimeFormat = RTC_HOURFORMAT12_AM; sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; sTime.StoreOperation = RTC_STOREOPERATION_RESET; HAL_RTC_SetTime(&hrtc, &sTime, FORMAT_BCD); sDate.WeekDay = RTC_WEEKDAY_MONDAY; sDate.Month = RTC_MONTH_JANUARY; sDate.Date = 0x1; sDate.Year = 0x15; HAL_RTC_SetDate(&hrtc, &sDate, FORMAT_BCD); /**Enable the WakeUp */ HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, RTC_WAKEUP_COUNTER, RTC_WAKEUPCLOCK_CK_SPRE_16BITS); RTC->ISR &= (~RTC_ISR_WUTF);}void EnterStopMode(void){ #if !defined( BASE_STATION ) if((MainState & (MainState_AcOk | MainState_Charging)) == 0){ MainState = (MainState_TypeDef)((MainState & 0xff00) | MainState_Stop); key_exti(); HAL_PWR_EnterSTANDBYMode(); } #endif}2016-01-12 5:13 AM
Hi cat.tom.002,
I recommend that you take a look to this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F437%20exiting%20standby%20incorrectly¤tviews=63]discussion which talks about a similar use case. As mentioned, you can be inspired form AN4538 ''“Power consumption optimization with STM32F3xx microcontrollers “ at thishttp://www.st.com/web/en/resource/technical/document/application_note/DM00121474.pdf
which can help you a lot in your hole application. You find AN4538 firmware at thishttp://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257872
.-Hannibal-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.