2015-11-23 5:57 AM
I am new to STm32 architecture. Trying to get the internal temperature sensor going. I am using a STm32L151VC microcontroller, STM32-QFP100 programmer adapter and IAR tool chain. I am trying to use the following code, but looks like ADC conversion is giving me some random value. Sometimes, it shows a random number between 600~700 ( which doesn't make sense as the hot calibration voltage is 626 at 100 degrees according to the data sheet), and the most other time variable AD_value shows 0. Any help/comment will be highly appreciated.
int main(void) { /* Configure PB.12 (ADC1 Channel18) or PF.10 (ADC1 Channel31) in analog mode -*/ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; /* Enable the GPIOB Clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Enable the HSI */ RCC_HSICmd(ENABLE); /* Wait until HSI oscillator is ready */ while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET); /* ADC1 Configuration -----------------------------------------------------*/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; // Set conversion data alignement ADC_Init(ADC1, &ADC_InitStructure); ADC_TempSensorVrefintCmd(ENABLE); /* Wait until ADC + Temp sensor start */ T_StartupTimeDelay = 1024; while (T_StartupTimeDelay--); /* Setup ADC common init struct */ ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div4; ADC_CommonInit(&ADC_CommonInitStructure); ADC_RegularChannelConfig(ADC1, ADC_Channel_16, 1, ADC_SampleTime_384Cycles); /* Start ADC1 Software Conversion */ while (1) { RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); ADC_Cmd(ADC1, ENABLE); /* Wait until the ADC1 is ready */ while(ADC_GetFlagStatus(ADC1, ADC_FLAG_ADONS) == RESET); ADC_SoftwareStartConv(ADC1); AD_value=ADC_GetConversionValue(ADC1); } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.