2016-04-24 2:27 AM
Hi,
I've build a program that runs fine, but IRQ are only fired when I start the µC with the debugger.Without the debugger, I can see that the µC runs correctly the program thanks to some blinking led, but none of my IRQ are firing.If I connect the debugger to the µC without downloading the program ( with ST-Link Utility for example), then I disconnect the debugger, IRQ are fired correctly.How can that be ???Thank you for your help.BR,Vincent.2016-04-24 5:10 AM
wrong program only.
2016-04-24 6:09 AM
I would double check you have enabled all the clocks you need, and the vector table address is set correctly. Review the startup up code related to external clocks, waiting for them and the PLL to start properly.
On the hardware side, review the states of the BOOTx pins.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.