2021-05-17 7:28 AM
Hello,
I am working with the discovery board STM32L100RC. I am trying to have three different timers (TIM2, TIM3, TIM4) as PWM. I'd like to do it's to have each timer ouput at '1' (3.3v) when a boolean variable is equal to '1' and at '0' (0V) when the same variable is equal to '0' .
Here's what I started to code for each timer :
static void MX_TIM2_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
htim2.Instance = TIM2;
htim2.Init.Prescaler = 1;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 15999;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
HAL_TIM_MspPostInit(&htim2);
}My question is the following one : how can we ask the timer to change its value according to a variable ?
Thank you in advance for you help,
Jay.
Solved! Go to Solution.
2021-05-17 8:14 AM
There's no way to tie a timer output to a variable so that it changes automatically when the variable changes value. You'll need to change the timer output via enabling/disabling or changing duty cycle manually when the variable changes.
2021-05-17 8:14 AM
There's no way to tie a timer output to a variable so that it changes automatically when the variable changes value. You'll need to change the timer output via enabling/disabling or changing duty cycle manually when the variable changes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.