2015-03-13 8:17 AM
Hello,
I'm running an STM32L151 at 32MHz and SPI BaudRate = fPCLK / 4. The device is an SPI Master, and tries to read a Slave as fast as possible. I'm using DMA TX and RX to speed up things. I can see the SPI clock running at 8Mbit/s clock, but I still get approx 1.5 µsec timeout between each transmitted byte, which in the end reduces the troughput to less than 4Mb/s Is there anything I can do to help reduce this latency ? Thanks for help. BR, Vincent.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.