2026-05-15 6:02 AM - last edited on 2026-05-15 6:10 AM by FBL
Is there a STM32N6 throughput test on the USB 2-480Mb happened.
I'm just curious because i'm getting a throughput on my design of
* 97 Mb
Just wondering what is a idealistic throughput to see if i need to edit something on my end or this is a expected throughput to get.
2026-05-15 6:56 AM
Hello @Brenden_PLUS
Throughput varies based on several conditions, such as the size of the buffer being sent, packet and USB controller state checking mechanisms used, and the duration of continuous transmission.
I have not tested throughput on STM32N6 specifically, but based on tests performed on STM32H7, 97 is a reasonable value.
BR
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.