2016-02-02 5:15 AM
Hello friends,
I use STM32L100C-Discovery Board and I tried to add some library with use Manage Run - Time Environment tools(KEIL uVision5). I want to use ADC and I can not see ADC library . I just added ''Startup'' in Device and ''Core,DSP'' in CMSIS. Normally, when I used STM32F4 board, I could add ''ADC, GPIO, Framework, RCC'' library but now I choosed STM32L100C target and there is Not enough library options.http://i.hizliresim.com/jVGoGj.jpghttp://i.hizliresim.com/yLrXa7.jpg #stm32l1 #discovery-boardWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.