2016-10-10 5:08 AM
I have a STM32L051K8T6 which I am running from a 1.8v supply to interface with a Quectel UG95 modem. Project produced with STM32CubeMX. Code is compiled with Keil uVision 5.21a.
The firmware continually reboots about every 5 seconds (no watchdog implemented). Debugging with Keil reveals that SystemClock_Config is very slow completing and that after completion HCLK frequency is 2MHz. I take this to indicate that HSI did not start and the system has substituted the MSI clock. Voltage scaling is set to Scale2 and SYSCLK is configured for a frequency of 8MHz This is the code void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit; HAL_PWREx_EnableUltraLowPower(); /* Enable the fast wake up from Ultra low power mode */ HAL_PWREx_EnableFastWakeUp(); /* Select HSI as system clock source after Wake Up from Stop mode */ __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_StopWakeUpClock_HSI); __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2); HAL_PWREx_DisableLowPowerRunMode(); RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.HSIState = RCC_HSI_DIV4; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_8; RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_4; HAL_RCC_OscConfig(&RCC_OscInitStruct); RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1); PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_RTC; PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2; PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1; PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE; HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit); HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK); HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0); HAL_NVIC_EnableIRQ(SysTick_IRQn); } I have checked STM32L0xx_hal_conf.h and this shows VDD_VALUE as 1800mV. The actual supply voltage is 1.803V. What have I missed out or done wrong? The original prototype used a STM32L051K8T7 which is the same processor but with extended operating temperature range and this works. I am assuming that it was a little more tolerant of the low voltage. #hsi #stm32l05xx #1.8v2016-10-10 8:49 AM
Review what is happening to the NRST line, and the power rail.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.