2015-08-18 1:36 AM
2015-08-18 2:07 AM
Solved by myself.
Ensure that Touch keys are marked as extended in tsl_conf.h and not basic!2015-08-19 6:32 AM
Hello,
There are two solutions to your problem:
•1st one: you modify the main.c file of the TouchSensing_Linear application example to simulate several touchkeys by defining some linear position ranges. •2nd one: you modify the following files tsl_conf.h, tsl_user.h, tsl_user.c and main.c to use the linear sensor as touchkeys. This solution is fine but you will certainly get some side effects (touch crosstalk and reduce sensitivity on the channel 0) due to the fact that the sensor layout is not appropriate.For the second solution, please find attached a working example. We will investigate if a such example can be added into the STM32Cube package.
There is currently no user manual specifically covering the TouchSensing library included into STM32Cube packages. There is onlythe UM1606 which is covering the STMTouchlibrary which is very closed to the one available into STM32CUbe packages.A new UM covering the TouchSensing Library is on-going and should be available within September.
Best Regards,Thierry,
________________ Attachments : TouchSensing_3Tkeys.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0gd&d=%2Fa%2F0X0000000bcS%2FVVZFWIaHCE8AJQoo5bRnU1gYP71ff8WoqYmjv3y7aHQ&asPdf=false2015-08-26 12:54 AM
Hello Thierry,
Thanks for the answer. I currently have 8ch and 8 banks Touchkeys. I would like to have cascade acquisition of all touchkeys (banks). I've done the following:#define TSLPRM_USE_ZONE (1) in tsl_conf.hTSL_tIndex_T MyBankSorting[TSLPRM_TOTAL_BANKS] = {0, 1, 2, 3, 4, 5, 6, 7};TSL_Zone_T MyZone = { MyBankSorting, 0, 8 // Number of Banks in the Zone}; In tsl_user.cIt seems as zone (cascade) is not working.Do I need to add this somewhere? TSL_acq_ZoneConfig(&MyZone, 0);
2015-09-08 10:29 AM
2015-09-09 6:58 AM
Hi a.alya,
What about the example provided by Thierry? Did you tested it?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-09-30 2:36 AM
Hi Mayla
I tested all the samples and it seems I found a solution On my side one bunk per channel works, If I assign a few channel to one bank it does not work. Also The are 20 state of touch sensor detection : TSL_StateId_enum_T Why only 2 works? I mean to detect a key pressing (in fact touching) I use TSL_STATEID_DETECT and TSL_STATEID_DEB_RELEASE_DETECT like #define TKEY_PRESSED(NB)\ ((MyTKeys[(NB)].p_Data->StateId == TSL_STATEID_DETECT) || \ (MyTKeys[(NB)].p_Data->StateId == TSL_STATEID_DEB_RELEASE_DETECT)) But all other states does not work. Why is that? I never get TSL_STATEID_TOUCH, for example as well as other states. So to detect a first touching, long touching I need to use my own additional triggers, flags etc.2017-04-04 3:40 PM
This does a pretty good job of explaining things:
Several states like 'TOUCH' require DXS (Detection Exclusion System) to be enabled in the
tsl_conf.h
file.Others like PROXIMITY require that to be enabled as well.
The state you are using TSL_STATEID_DEB_RELEASE_DETECT isn't a real good one to use. That state is when it is in debouncing, meaning 'I MIGHT' have a release happening. If the number of release detections passes the DEBOUNCE setting, then that state will transition to a solid RELEASE state.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.