2018-11-22 12:58 AM
Dear STM32 Members,
I have read a value from ADC,
Is there anyway that I can display ADC result to my scope without DAC?
Any clues guys ?
Thanks and kind regards,
2018-11-22 1:04 AM
Hi there,
A basic method would be to have a timer running in PWM mode with the reload register set to the maximum resolution of the ADC and then copy the ADC result to the compare register of the timer. Then all you have to do is to measure the ON time of the PWM with the scope.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.