2014-09-30 3:11 AM
Hi,
I'm using an STM32L051 microcontroller for a low power application. Actually I am working on a state change between low power and normal operating mode. Therefore I am trying to switch the system clock to PLL but it seems the RCC_CFGR register is read-only for some unknown reasons. I am using the HAL library and the following initialization sequence (directly copied from the examples):RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct; /* Enable Power Control clock */ __PWR_CLK_ENABLE(); /* The voltage scaling allows optimizing the power consumption when the device is clocked below the maximum system frequency, to update the voltage scaling value regarding system frequency refer to product datasheet. */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); /* Enable HSI Oscillator and activate PLL with HSI as source */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSEState = RCC_HSE_OFF; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4; RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2; RCC_OscInitStruct.HSICalibrationValue = 0x10; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) ErrorHandler(); /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) ErrorHandler(); After this sequence the RCC_CFGR:SW bits are switched to HSE (0b11), RCC_CFGR:SWS is HSI (0b01) and RCC_CFGR:PLLSRC is switched to HSE allthough HSE is deactivated and NO external clock source is available. Manual writing to the CFGR register does not change the value. NOTE: There was no other initialization prior to this sequence. 1. Any ideas what's going wrong? 2. Under which conditions are the RCC registers locked (except the backup domain stuff)? Thanks in advance, Carsten Schumann Prior to this2014-09-30 4:05 AM
Issue is solved and was related to a non-L0 aware debugger in conjunction with changed register addresses from L1->L0.
@Moderator: Please delete the thread, since the request is invalid. CarstenWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.