2014-10-04 9:34 AM
Hi people,
I'm new in STM's world!Thanks to this forum, I made the USB - UART connection on STM32L-Discovery.Now, I have to test speed communication with a byte array of max 20 bytes.I use STM32_USB-FS-Device_Lib, example virtual_COM_port for stm32l-eval. Can someone help me with code to inizialize and send an array via uart-usb and vice-versa?Sorry for my bad english!Thank you all!2014-10-09 2:12 PM
Hi Guys,
can sameone help me??? Do you need more explanations about my project?? Thanks for help....2014-10-09 2:33 PM
Do you need more explanations about my project??
The pool is pretty shallow here, if the project has a budget consider some of the contractors. ST maintains a list of consultants and contractors.http://www.st.com/web/en/support/mcu_design_consultants.html
2014-10-10 11:11 AM
Thanks Clive...
Unfortunately
I have no
budget.
I'm just a
beginning student
with this card
,for educational purposes
.I thought
someone had
already
had experience with
this type of connection
, though not
with
this
exact
card
.I
just
need some guidance
,maybe
from someone who has
used
these libraries
,where to insert
a function
in a loop
sending each
byte
on the other side
(via USB
to
UART
or
UART
to
USB)
?
2014-10-11 11:05 AM
''I'm just a
beginning student
...I
just
need some guidance''
And that is what your teachers & tutors are there for!If you're stuck with your course work, those are really the people you should be going to for help.2014-10-14 12:41 PM
So OK.
thank you allanyway!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.