2018-06-20 9:58 PM
Another issue found, potentially in HAL drivers (HAL_RCCEx_PeriphCLKConfig):
I try to use PLL3R for I2C clock:
PeriphClkInitStruct.I2c123ClockSelection = RCC_I2C123CLKSOURCE_PLL3; //USB will FAIL!!!
If I do this - my
USB is dead
(using also PLL3, PLL3Q):PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL3;
It works just with:
PeriphClkInitStruct.I2c123ClockSelection = RCC_I2C123CLKSOURCE_D2PCLK1;
Conclusion:
it looks like a bug in HAL driver functions:
if a PLL output is used as clock source, even they have 3 clock outputs for peripherals (P, Q, R):
==> JUST
ONE
PLL clock output can be used for peripherals!or: if more then one 'or-ed' macros for same PLL are not zero - just one config seems to win (or they kill each other).So, you CANNOT use a PLL with
MORE THEN ONE
clock output for peripheral clocks!(similar to the same issue with SDMMC1: it cannot use PLL2 - if PLL2 is already used for SPI clocks, the HAL driver code (or chip ?) seems to make it exclusive to 'just one PLL clock output is usable').
2018-06-21 7:54 AM
So if you program the RCC registers and avoid the Cube/HAL contraptions, does it work as expected?
JW
2018-06-21 9:31 AM
Hi
Jaekel.Torsten
,I confirm that there is an issue with RCC driver in the STM32CubeH7 package.
It is a similar issue to the one you have already reported in
https://community.st.com/0D50X00009XkhUQSAZ
.A patch is provided in
https://community.st.com/0D50X00009XkZJxSAN
.Could you please apply it at your end, waiting for the official fix in the next STM32CubeH7 version?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-06-21 1:26 PM
Thank you, Amel, I appreciate.
I found and will take the errata. Great.
Many regards, Torsten
2018-07-26 5:53 AM
Fix deployed in STM32CubeH7 v1.3.0 currently available on the web.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.