2020-11-12 1:51 AM
Hello,
this is a description of PLL settings from a reference manal
00: The PLL1 input (ref1_ck) clock range frequency is between 1 and 2 MHz (default after reset)
01: The PLL1 input (ref1_ck) clock range frequency is between 2 and 4 MHz
10: The PLL1 input (ref1_ck) clock range frequency is between 4 and 8 MHz
11: The PLL1 input (ref1_ck) clock range frequency is between 8 and 16 MHz
What should I set if my PLL input is exactly at the boundary? Eg 8MHz.
BR
Jan
2020-11-12 3:59 AM
Choose depending on the real frequency 8.000001 or 7.999999 <joke> . Choose any, it should not matter.
2020-11-12 4:14 AM
Thanks for reply. I know that both is working :)
Do you know, what these settings actually do and what happens if the difference would be bigger?
2020-11-12 5:20 PM
PLL is a semi-analog circuit, especially the phase-detector and subsequent filter. There's tradeoff between lock time, jitter and stability in its design. I'd say, this parameter controls this part of the PLL, setting it to a tested optimal state for given input frequency.
> what happens if the difference would be bigger?
Probably the parameters given in DS won't be met under all possible circumstances (power supply voltage range, temperature range).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.