2025-04-23 12:14 AM - edited 2025-04-23 1:06 AM
Hello,
I have a question about the usage of the MCE in the STM32H7RS
I have the STM32H7S78-DK board
I'm starting with a project that show images to LTDC with images on the flash (copy with DMA2D) and the framebuffer is on the PSRAM.
My project works with this tuto to get the flash running : https://github.com/ST-TOMAS-Workshop/stm32h7s_workshop/tree/main/1_external_memory
And this one to have MCE working : https://github.com/ST-TOMAS-Workshop/stm32h7s_workshop/tree/main/3_external_memory_encryption
The project seems to run well beacause my led blink like it should but !
defining my images in "const uint16_t ecran_start" now (since MCE is enable) gives me black images (in debug session i see the variable in Expressions correctly) .
Removing the const the images shows but by internal ram will be filled very quick
Putting the image in my PSRAM section it is glitched on the screen
My framebuffer is in PSRAM and works because DMA2D show a red rectangle that i programmed (DMA2D R2M)
Putting framebuffer into internal RAM doesn't fix issues
Is there special things to setup about memory usage with MCE ?
Thanks
Solved! Go to Solution.
2025-05-14 6:52 AM
Hello @Hamady,
I'm under investigation.
When I tested your project, I got an error message from debugger back end.
Did you configure the memory in memory mapped mode before using the MCE?
I didn't find the memory mapped configuration in your code.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-14 11:48 AM
hello @KDJEM.1
This is normal that i dont use memory mapped mode
my flash is configured as the workshop (XIP and after MCE ) of the H7S7 suggested so no memory mapped.
And my PSRAM doesn't need MCE as we just need the flash to be encrypted
Tell me if you need more info
Thanks
2025-05-20 7:26 AM
Hello, @KDJEM.1
Do you have any news about the issue.
Thanks
2025-07-06 6:10 AM
For info i found the ISSUE
Put this in the boot file
pConfig.PrivilegedAccess=MCE_REGION_NPRIV;
In the tutorial if you put the default line in the boot all peripheral will be disabled
pConfig.PrivilegedAccess=MCE_REGION_PRIV //wrong line
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.