2025-04-11 10:09 AM - last edited on 2025-04-11 10:26 AM by mƎALLEm
I have a problem with an STM32H7A3 which remains stuck in SystemClock_Config. I use Keil. Any ideas please?
it just remain stucked here:
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/*AXI clock gating */
RCC->CKGAENR = 0xFFFFFFFF;
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = 64;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 42;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 4;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2025-04-11 12:07 PM - edited 2025-04-11 12:08 PM
LSI (Low Speed Internal)
Really shouldn't have a lot of dependencies. I'd check the supplies (VDD, VDDA), and things like the VCAP voltage and capacitors placed there. Likely need a total of about 4.7uF, and see about 1.25V
Check where the LSI is powered, ie which domain
Check netlists, for islands where power might not reach due to naming or connectivity.
Can you share a salient portion of the schematic?
2025-04-11 12:12 PM
Not sure where the LSI ready loop code is situated, but shouldn't be issues related to LSE external crystal and capacitance/resistance..
Perhaps compile with Optimization OFF, so we can identify the specific code failing
2025-04-11 12:15 PM
@Tesla DeLorean wrote:
Not sure where the LSI ready loop code is situated, but shouldn't be issues related to LSE external crystal and capacitance/resistance..
Perhaps compile with Optimization OFF, so we can identify the specific code failing
He said, it's working with LSI but not with LSE:
"It was stuck in LSE so I just changed from LSE to LSI and is working now".
He didn't share his code with LSI.
2025-07-15 6:37 AM
@mƎALLEm wrote:
@laurianus wrote:
This was generated like this by STM32 Cube MX
In that case, I need to escalate that internally. Could you please share your ioc file?
Issue fixed in the CubeMx 6.15.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.