2021-09-06 5:20 AM
Is there any sample project that can guide in configuring touch screen functionality on the VGA LCD in STM32H753I-EVAL2 board. As of now, I have not found any relevant documentation regarding the same.
2021-09-06 6:19 AM
/* Initialize the Touch screen */
BSP_TS_Init(640, 480);
These examples are available
STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Applications\STemWin\STemWin_SampleDemo\Core\Src\main.c
STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Demonstrations\STemWin\Core\Src\k_bsp.c
STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Examples\BSP\Src\main.c
STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Examples\BSP\Src\touchscreen.c
STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Examples\BSP\Src\ts_calibration.c
2021-09-06 10:48 PM
Thank you for these examples.
Also, there is no mention about which touch screen driver is used for the 5.7" 640x480 Ampire LCD display. Is it TS3510 or EXC7200?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.