STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nuclel STM32F303K8 TIM2 as Encoder

I'm working to read 2 identical encoders from 2 identical motor drivers.I use TIM2 and TIM3 to read the encoders.The encoder at TIM3 works properly, but the encoders at TIM2, I could see in debug mode the IRQ but the register CNT is zero. But every t...

FTrom by Associate II
  • 1637 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H745 SDMMC DMA Rx Overrun/Tx Underrun

Hi,I am working on STM32H745 discovery board and trying to configure the onboard 4GB eMMC flash over SDHC1 interface. I am loading default discovery board configuration by the CubeMx configuration, which sets both M7 and M4 and all AHB buses to run a...

Joyabb by Associate II
  • 4013 Views
  • 3 replies
  • 0 kudos

how to protect analog inputs ?

I've seen the discussion in an old question herehttps://community.st.com/s/question/0D50X00009XkbAd/how-to-protect-analog-inputs-Accordingly, ADC inputs are not 5v tolerant in ADC mode.I started studying some Zener diodes, in particular 1n4727 Vz 3vh...

andrewg by Associate III
  • 3858 Views
  • 4 replies
  • 0 kudos

STM32H753I-EVAL2 touch screen functionality

Is there any sample project that can guide in configuring touch screen functionality on the VGA LCD in STM32H753I-EVAL2 board. As of now, I have not found any relevant documentation regarding the same.

hrm2519 by Associate II
  • 1450 Views
  • 2 replies
  • 0 kudos

How to program using VIM + GCC on STM32F415?

Hi, I'm a complete noob, coming from Arduino (MCU: ATmega328p) Board and I want to have similar programming environment there.General information:OS: LinuxMCU: STM32F415Board: custom one which has USB Mini B portI would like to use GCC + VIM if possi...

0xZER0 by Associate II
  • 4432 Views
  • 3 replies
  • 1 kudos

stm32h750 qspi bank 2 only

Can I use a external flash in qspi mode connected to qspi peripheral bank 2 ?I wan to test 2 things:Dump code from ext flash to sram partition to execute appExecute in place code in ext flash I use bank2 because in lqfp 100 package i had direct and c...

JCuna.1 by Senior
  • 947 Views
  • 1 replies
  • 0 kudos

Lossless data processing

Hello,I'm working with STM32F410RB , My question is not related to code but it's architectural. I'm using DMA uart to communicate with another device, i noticed that dma buffer change its content before my code processing the data. So i'm loosing som...

Ahajr.1 by Associate II
  • 1670 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.