2020-01-02 8:03 AM
Looking for confirmation that the SDRAM data bits can be swapped within their byte lanes (D15..D8, D7..D0) to reduce the routing complexity. We are using vanilla SDRAM (non-DDR), specifically the ISSI IS42S32800G.
Thanks.
2020-01-02 8:16 AM
Yes I believe you could do that, you would need to apply the same bit swizzling to the configuration word(s) written to the memory IC.
2020-01-02 8:22 AM
Thanks for the quick reply. I believe the chip configuration (mode register) is written using the address pins alone, but would welcome any input on that as well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.