2021-06-25 2:10 AM
Hi
Does anyone know if on STM32H753, Can the master clock output ( MCLK output) work if the I2S mode is set as slave?
Thanks
Sam
2021-06-25 2:32 AM
MCK Generation
The master clock MCK can be generated regardless to the SPE bit. The MCK generating is controlled by the following bits:
– I2SMOD must equal to 1,
– I2SCFG must select a master mode,
– MCKOE must be set to 1
Is there anyway to get around this? or if its a hardware level implementation that limits this?
Many thanks!
2021-06-26 2:11 AM
This is given by hardware.
Can't you generate the clock on that point in another way, e.g. isn't that pin also output of a timer?
JW
2021-07-17 8:17 AM
As always... Instead of SPI/I2S peripheral try using SAI peripheral.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.