STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Inaccurate PWM Freq

I have the Nucleo - STM32F446RE board and have been trying to work with the PWM (using CubeMX) on it for Motor Control. But for some reason I was getting 32.8Khz whenever I set it for 32Khz (while SYSCLK was 180Mhz). I checked my calculations but to ...

0693W00000BbSjCQAV.png

Resolved! Incorrect time elapsed using SysTick

Hi, I'm currently using STM32F401RE Nucleo-64 Board. My purpose of this project is to configure ISM330DLC Accelerometer, taking reference from STEVAL-BFA001V1B sample code on Vibration Analysis. As a summary:After enabling the accelerometer FIFO FULL...

ZTan.2 by Associate II
  • 3394 Views
  • 4 replies
  • 1 kudos

Resolved! External load capacity calculation

Hello All,I'm a bit stuck on the calculation of the external load capacitances on a STM32F205, regarding the LSE Oscillator for 32.768kHz.In the AN2867 there is the following formula:When assuming that CL1 and CL2 are the same, the formula could be s...

0693W00000BceheQAB.png 0693W00000Bcei3QAB.png
ame by Associate II
  • 5877 Views
  • 7 replies
  • 0 kudos

Availability of STM32 controller

Hello Support Team,I am looking for support regarding controller. I want to use STM32H745IIT6 in my design. I have completed my almost design and when I want to purchase this controller I found it non stock.Can you please let me know the availability...

NJani.2 by Associate II
  • 1832 Views
  • 3 replies
  • 0 kudos

Stm32f407vg don't work with SD card via SPI.

I am beginner and I want to read/write data to SD card via SPI.I do everything according to this instruction https://01001000.xyz/2020-08-09-Tutorial-STM32CubeIDE-SD-card/ and all time get f_getfree error (3)And I also tried to repeat by this instruc...

DK.7 by Senior
  • 878 Views
  • 0 replies
  • 0 kudos

STM32F4 input capture Confusion.

 Hi.I’m working on a Nucleo-411, using CubeIDE, and HAL, and I want to read 4 PWM signals from am RC receiver. That is 4 50Hz signals, with a pulse width ranging from 0.5mS to 2.5mS. I’m following the reference manual, and some examples, and so far I...

CPetr.1 by Associate II
  • 3504 Views
  • 6 replies
  • 0 kudos

How to clear FDCAN error callback?

Hello, I would like to use the error callback of the FDCAN module on the STM32H743ZI and so far I got it working. Once an error (e.g protocol error) occured the callback keeps getting called. According to the reference manual an interrupt flag can be...

MLang.7 by Associate III
  • 5304 Views
  • 4 replies
  • 0 kudos

Resolved! ADC on NUCLEO-F446RE very noisy, some suggestions are needed.

Hi all!I'm developing on a evaluation board NUCLEO-F446RE STM32 F4.I've to read an adc input in order to monitor a battery.There's a lot of unexpected noise in my acquired data, as visibile in attahments.I've tied directly the adc input to Vref and t...

0693W00000CzsUAQAZ.png 0693W00000CzsTgQAJ.png
GStra.1 by Associate II
  • 1709 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.