2023-10-30 9:41 AM
Hello,
I use the STM32H750VBT6, I have a problem when I use the ADC's DMA with 16-bit resolution (but not only).
The input analog signal varies from 0 to 3v, but the minimum converted value is 20000 (out of 65000).
It's as if the ADC isn't using the entire input range, do you have any idea where the problem comes from?
Paul
Parameters :
ADC 16/12 bits resolution
Continuous Conversion Mode
End of Single Conversion
DMA One Shot Mode
Solved! Go to Solution.
2023-10-30 10:33 AM
Custom board? Check for valid power connections on VDD/VDDA/VSS/VSSA pins. Check for proper supply and decoupling at VREF+ pin. If it's a high impedance source, ensure your sampling time is sufficient. Ground the signal directly to GND and see what the reading is. 20000 is quite a bit above ground so I feel like something else is happening.
2023-10-30 10:33 AM
Custom board? Check for valid power connections on VDD/VDDA/VSS/VSSA pins. Check for proper supply and decoupling at VREF+ pin. If it's a high impedance source, ensure your sampling time is sufficient. Ground the signal directly to GND and see what the reading is. 20000 is quite a bit above ground so I feel like something else is happening.
2023-10-31 1:46 AM
Thank you for your reply
I use the Adafruit 5032 developer board (https://www.digikey.fr/fr/products/detail/adafruit-industries-llc/5032/15204086). So normally the power supplies are well wired but I'll check it out. When I put the signal directly on GND I get values close to 18500 with 16-bit resolution. But with 12-bit resolution, the minimum value connected to GND is close to 600.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.