2023-08-11 4:37 AM
The SPI2_MISO pin (PI2) at the arduino connector of the STM32H745XI board was accidentally connected to the MOSI of another SPI device giving around 5V and now the board red LED (LD3) keeps being on...According to the user manual, this means STLK Over Current.
In the FAIL.TXT file: The interface firmware FAILED to reset/halt the target MCU
Is there a way to fix that?
I am afraid that the Core is permanently damaged??
Solved! Go to Solution.
2023-08-11 4:40 AM
2023-08-11 4:40 AM
2023-08-11 5:36 AM
Try to recover the board with STM32CubeProgrammer. Do chip erase.
If it doesn't work then connect BOOT0 pin to 3.3 V, connect board to STM32CubeProgrammer and perform chip erase.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.